VF65GS10 power design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VF65GS10 power design

ソリューションへジャンプ
2,122件の閲覧回数
RsBogdan
Contributor I

SR Number: 1-1093845751
Date Opened: 17-Jul-2013 03:57:42 PM
Subject: VF65GS10 power design
Description: Customer is currenlty desiging with VF65GS10 and was aware that theVF65GS10 tower board was delayed to production. Rumor is that there was an issue in the power solution for this board .. the customer would like to know any details so that they dont have the same issue.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,984件の閲覧回数
naoumgitnik
Senior Contributor V

Dear RsBogdan,

Below is an excerpt from the older 'Re: About the issue of TWR-VF65GS10 power supply circuit' thread:

  1. If your customer does not use USB as a power source, all the below information is irrelevant.
  2. The issue was with a type of the previously used Switch IC controlling the USB power on the board - MIC2026, whose built-in current threshold appeared to be marginal for the latest SW applications, so it had to be replaced with a drop-in replacement, MIC2506, with a higher threshold.
  3. The next schematic revision (in progress) with MIC2506 instead of MIC2026 will be G1.

Best regards, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,985件の閲覧回数
naoumgitnik
Senior Contributor V

Dear RsBogdan,

Below is an excerpt from the older 'Re: About the issue of TWR-VF65GS10 power supply circuit' thread:

  1. If your customer does not use USB as a power source, all the below information is irrelevant.
  2. The issue was with a type of the previously used Switch IC controlling the USB power on the board - MIC2026, whose built-in current threshold appeared to be marginal for the latest SW applications, so it had to be replaced with a drop-in replacement, MIC2506, with a higher threshold.
  3. The next schematic revision (in progress) with MIC2506 instead of MIC2026 will be G1.

Best regards, Naoum Gitnik.

0 件の賞賛
返信