VF6 and 8bit-NAND Flash memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VF6 and 8bit-NAND Flash memory

Jump to solution
2,393 Views
george
Senior Contributor II

Hi all,

I wish to connect VF6 series and 8bit-NAND of Vybrid.

However, it is not known whether it is correct to use which 8 bits of NF_IO [15:0].

Is my understanding correct although it seems that NF_IO [7:0] is correct?

Best Regards,

George

Labels (3)
Tags (5)
0 Kudos
Reply
1 Solution
2,132 Views
naoumgitnik
Senior Contributor V

Dear George,

Below are excerpts from the NAND FLASH operation descriptions:

  • "This 8-bit bus acts as a multiplexed bus to transfer data, address, and instructions."
  • " Bidirectional 8-bit multiplexed bus used to send data/command/address to their respective registers in the NAND flash device. The data read from the NAND flash device is also available on these lines."
  • "For 16-bit devices, commands and addresses use the lower 8 bits (7:0). The upper 8 bits of the 16-bit data bus are used only during data-transfer cycles."
  • Etc.

So, it is the lower 8 bits; they are always used - for both 8- and 16-bit devices.

Sincerely, Naoum Gitnik.

View solution in original post

0 Kudos
Reply
2 Replies
2,133 Views
naoumgitnik
Senior Contributor V

Dear George,

Below are excerpts from the NAND FLASH operation descriptions:

  • "This 8-bit bus acts as a multiplexed bus to transfer data, address, and instructions."
  • " Bidirectional 8-bit multiplexed bus used to send data/command/address to their respective registers in the NAND flash device. The data read from the NAND flash device is also available on these lines."
  • "For 16-bit devices, commands and addresses use the lower 8 bits (7:0). The upper 8 bits of the 16-bit data bus are used only during data-transfer cycles."
  • Etc.

So, it is the lower 8 bits; they are always used - for both 8- and 16-bit devices.

Sincerely, Naoum Gitnik.

0 Kudos
Reply
2,132 Views
george
Senior Contributor II

Thanks Naoum,

BR

Fukutomi

0 Kudos
Reply