VF6 and 8bit-NAND Flash memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VF6 and 8bit-NAND Flash memory

ソリューションへジャンプ
2,371件の閲覧回数
george
Senior Contributor II

Hi all,

I wish to connect VF6 series and 8bit-NAND of Vybrid.

However, it is not known whether it is correct to use which 8 bits of NF_IO [15:0].

Is my understanding correct although it seems that NF_IO [7:0] is correct?

Best Regards,

George

ラベル(3)
タグ(5)
0 件の賞賛
返信
1 解決策
2,110件の閲覧回数
naoumgitnik
Senior Contributor V

Dear George,

Below are excerpts from the NAND FLASH operation descriptions:

  • "This 8-bit bus acts as a multiplexed bus to transfer data, address, and instructions."
  • " Bidirectional 8-bit multiplexed bus used to send data/command/address to their respective registers in the NAND flash device. The data read from the NAND flash device is also available on these lines."
  • "For 16-bit devices, commands and addresses use the lower 8 bits (7:0). The upper 8 bits of the 16-bit data bus are used only during data-transfer cycles."
  • Etc.

So, it is the lower 8 bits; they are always used - for both 8- and 16-bit devices.

Sincerely, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,111件の閲覧回数
naoumgitnik
Senior Contributor V

Dear George,

Below are excerpts from the NAND FLASH operation descriptions:

  • "This 8-bit bus acts as a multiplexed bus to transfer data, address, and instructions."
  • " Bidirectional 8-bit multiplexed bus used to send data/command/address to their respective registers in the NAND flash device. The data read from the NAND flash device is also available on these lines."
  • "For 16-bit devices, commands and addresses use the lower 8 bits (7:0). The upper 8 bits of the 16-bit data bus are used only during data-transfer cycles."
  • Etc.

So, it is the lower 8 bits; they are always used - for both 8- and 16-bit devices.

Sincerely, Naoum Gitnik.

0 件の賞賛
返信
2,110件の閲覧回数
george
Senior Contributor II

Thanks Naoum,

BR

Fukutomi

0 件の賞賛
返信