VF5xx/USB Control Register (USBC0_CTRL) address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

VF5xx/USB Control Register (USBC0_CTRL) address

跳至解决方案
2,005 次查看
soichiyamamoto
Contributor V

Hi

Is USB Control Register (USBC0_CTRL) address a 0x4003_5800  or 0x4003_4800?

It is written as USB Control Register (USBC0_CTRL)  :0x4003_5800 in VYBRIDRM.pdf/2143page.

But, It is USB Control Register (USBC0_CTRL):0x4003_4800 in IAR EWARM.

Best regards,

soichi

标签 (1)
0 项奖励
回复
1 解答
1,797 次查看
kef2
Senior Contributor V

0x40034800 seems working properly. Table 3-2 Peripheral bridge 0 slot assignment tells that 0x4003_4000 slot is used for USBC0 and 0x4003_5000 slot is not used.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,798 次查看
kef2
Senior Contributor V

0x40034800 seems working properly. Table 3-2 Peripheral bridge 0 slot assignment tells that 0x4003_4000 slot is used for USBC0 and 0x4003_5000 slot is not used.

0 项奖励
回复
1,797 次查看
soichiyamamoto
Contributor V

Dear TIC team,

Is mention of VYBRIDRM.pdf/2143page an error in writing of Manual?

If it is an error of Manual, please revise Manual.

Best Regards,

soichi

0 项奖励
回复
1,797 次查看
naoumgitnik
Senior Contributor V

Thanks for your help, kef!

Soichi,

I marked this typo in the Reference Manual to fix it in the next revision. - Thanks for finding it!

Sincerely, Naoum Gitnik.

0 项奖励
回复
1,797 次查看
soichiyamamoto
Contributor V

Dear Edward,

Thank you for reply.

Sorry,

Best Regards,

soichi

0 项奖励
回复