VF5xx/USB Control Register (USBC0_CTRL) address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VF5xx/USB Control Register (USBC0_CTRL) address

Jump to solution
1,985 Views
soichiyamamoto
Contributor V

Hi

Is USB Control Register (USBC0_CTRL) address a 0x4003_5800  or 0x4003_4800?

It is written as USB Control Register (USBC0_CTRL)  :0x4003_5800 in VYBRIDRM.pdf/2143page.

But, It is USB Control Register (USBC0_CTRL):0x4003_4800 in IAR EWARM.

Best regards,

soichi

Labels (1)
0 Kudos
Reply
1 Solution
1,777 Views
kef2
Senior Contributor V

0x40034800 seems working properly. Table 3-2 Peripheral bridge 0 slot assignment tells that 0x4003_4000 slot is used for USBC0 and 0x4003_5000 slot is not used.

View solution in original post

0 Kudos
Reply
4 Replies
1,778 Views
kef2
Senior Contributor V

0x40034800 seems working properly. Table 3-2 Peripheral bridge 0 slot assignment tells that 0x4003_4000 slot is used for USBC0 and 0x4003_5000 slot is not used.

0 Kudos
Reply
1,777 Views
soichiyamamoto
Contributor V

Dear TIC team,

Is mention of VYBRIDRM.pdf/2143page an error in writing of Manual?

If it is an error of Manual, please revise Manual.

Best Regards,

soichi

0 Kudos
Reply
1,777 Views
naoumgitnik
Senior Contributor V

Thanks for your help, kef!

Soichi,

I marked this typo in the Reference Manual to fix it in the next revision. - Thanks for finding it!

Sincerely, Naoum Gitnik.

0 Kudos
Reply
1,777 Views
soichiyamamoto
Contributor V

Dear Edward,

Thank you for reply.

Sorry,

Best Regards,

soichi

0 Kudos
Reply