Using OpenVG with 2D ACE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using OpenVG with 2D ACE?

Jump to solution
2,126 Views
johnhom
Contributor III

Hello.

When using using OpenVG on Vybrid, can we route the output to a memory-mapped frame buffer and feed that as a layer into the 2D ACE, making use of its composition capabilities and layers? Or is it that the OpenVG output always outputs to the display?

Tags (3)
1 Solution
1,820 Views
johnhom
Contributor III

Thanks for the suggestion for moving the post. I thought I had opened it in the Vybrid Processors Community Place, but anyway I've moved it now.

My colleague has answered my question, and the answer is yes, the OpenVG output can be used as an input to the 2D ACE for composition with other layers.

View solution in original post

0 Kudos
Reply
2 Replies
1,820 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Vybrid Processors ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community. 

0 Kudos
Reply
1,821 Views
johnhom
Contributor III

Thanks for the suggestion for moving the post. I thought I had opened it in the Vybrid Processors Community Place, but anyway I've moved it now.

My colleague has answered my question, and the answer is yes, the OpenVG output can be used as an input to the 2D ACE for composition with other layers.

0 Kudos
Reply