Unable to see LEDs change on TWR-VF65GS10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to see LEDs change on TWR-VF65GS10

Jump to solution
2,188 Views
Keith4DSmith
Contributor V

Took TWR-VF65GS10 board out of box. Plugged USB cable into J3, in standalone mode, no tower. Power LED is on.

As per instructions, step 5 'Tilt the Board', I don't see the LEDs change.

Try to setup a terminal program with the COM port created by the VF board, no activity on the COM port.

Try to debug a Hello word program via IAR and OSJtag, no connection found.

Jungo/Windriver, ver. 10.1.0.0 driver running. COM14 device available via OpenSDS - CDC Serial Port, version 1.1.2600.1. Drive E: TW-VF65GS is present.

If hold RESET button down while connecting to J3 and release RESET, see BOOTLOADER.

What have I not done or have done wrong?

Labels (3)
0 Kudos
Reply
1 Solution
1,966 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
3 Replies
1,967 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,967 Views
Keith4DSmith
Contributor V

When using IAR, one does not use PE Micro debugger, one uses the CMSIS DAP debugger.

Follow these steps as supplied by IAR.

1) disconnect the USB cable from the TWR-VF65GS10 if it has

   been connected,

2) run and install the EWARM's .\arm\drivers\pemicro\PEDrivers_install.exe,

3) press and hold the reset button of the TWR-VF65GS10 until

   you have reconnected the USB cable to its OpenSDA/Micro-USB

   connector (J3)

4) copy the EWARM's .\arm\drivers\pemicro\OpenSDA\CMSIS-DAP_OpenSDA.S19

   file into the drive E: TWR-VF65GS,

5) disconnect and reconnect the USB cable,

6) set your project's workbench menu "Project>Options>Debugger>

Setup>Driver" to "CMSIS DAP" and "Project>Options>CMSIS DAP>

JTAG/SWD>Interface" to "SWD",

This setup powers the Vybrid controller via the USB cable connected to J3.

0 Kudos
Reply
1,967 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

The Tower systems comes with a micro SD memory you have to plug into the TWR SD connector.

The SD contains the binary image. Also please make sure the jumpers are configured correctly.

Best Regards,

Alejandro