USB1 port only powered

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB1 port only powered

Jump to solution
1,993 Views
juandiaz
Contributor II

I am intented to use only the USB1 port, Vybrid VF6xx. Is it totally necessary to power the VBUS and VBUS_DETECT of USB0 in order to use the USB1?

Labels (1)
Tags (3)
1 Solution
1,856 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to Table 17 (Recommended connections for unused analog interfaces)

of "Hardware Development Guide for Vybrid Family of MCUs, User’s Guide, Rev. 1, 05/2015".

http://cache.nxp.com/files/microcontrollers/doc/user_guide/VYBRIDHDUG.pdf?fsrch=1&sr=1&pageNum=1 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,857 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to Table 17 (Recommended connections for unused analog interfaces)

of "Hardware Development Guide for Vybrid Family of MCUs, User’s Guide, Rev. 1, 05/2015".

http://cache.nxp.com/files/microcontrollers/doc/user_guide/VYBRIDHDUG.pdf?fsrch=1&sr=1&pageNum=1 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------