USB LDO Specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB LDO Specification

Jump to solution
7,966 Views
markwatson
Contributor III

We are seeing some intermittent failures with the USB communication between our device (MVF61NS151...) and a host PC.  I started investigating and noted that the USB Dcap voltage is about 2.7 volts.  The tower board schematic labels this as 3V3 and the VYBRIDFSERIESEC on page 30 shows it as 3p0.  What is the correct voltage for the internal regulator for USB?  My bus voltage is at least 4.9 V, so that is not the problem.  Is there a register setting to disable the internal regulator?  I have no loads on the Dcap piin, just a couple of capacitors.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
7,654 Views
timesyssupport
Senior Contributor II

Hello Mark,

Thanks for following up with this; we have a ticket reporting the exact same issue/fix in our support queue and will be addressing this in our 3.13 Vybrid kernel support. Though not stated here, is it correct to assume this is while running the Timesys Vybrid kernel?

Thank you,

Timesys Support

View solution in original post

0 Kudos
Reply
5 Replies
7,654 Views
markwatson
Contributor III

I have determined that this is intended to be 3.0 V.  The Linux kernel was not enabling the regulator in the ANADIG section in the ANADIG_REG_3P0 register. The lowest order bit must be set. 

0 Kudos
Reply
7,655 Views
timesyssupport
Senior Contributor II

Hello Mark,

Thanks for following up with this; we have a ticket reporting the exact same issue/fix in our support queue and will be addressing this in our 3.13 Vybrid kernel support. Though not stated here, is it correct to assume this is while running the Timesys Vybrid kernel?

Thank you,

Timesys Support

0 Kudos
Reply
7,654 Views
karina_valencia
NXP Apps Support
NXP Apps Support

markwatson please answer previous question from Timesys

0 Kudos
Reply
7,654 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you  review this case?

0 Kudos
Reply
7,654 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport do you have an update?

0 Kudos
Reply