USB LDO Specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB LDO Specification

ソリューションへジャンプ
7,792件の閲覧回数
markwatson
Contributor III

We are seeing some intermittent failures with the USB communication between our device (MVF61NS151...) and a host PC.  I started investigating and noted that the USB Dcap voltage is about 2.7 volts.  The tower board schematic labels this as 3V3 and the VYBRIDFSERIESEC on page 30 shows it as 3p0.  What is the correct voltage for the internal regulator for USB?  My bus voltage is at least 4.9 V, so that is not the problem.  Is there a register setting to disable the internal regulator?  I have no loads on the Dcap piin, just a couple of capacitors.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
7,480件の閲覧回数
timesyssupport
Senior Contributor II

Hello Mark,

Thanks for following up with this; we have a ticket reporting the exact same issue/fix in our support queue and will be addressing this in our 3.13 Vybrid kernel support. Though not stated here, is it correct to assume this is while running the Timesys Vybrid kernel?

Thank you,

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
7,480件の閲覧回数
markwatson
Contributor III

I have determined that this is intended to be 3.0 V.  The Linux kernel was not enabling the regulator in the ANADIG section in the ANADIG_REG_3P0 register. The lowest order bit must be set. 

0 件の賞賛
返信
7,481件の閲覧回数
timesyssupport
Senior Contributor II

Hello Mark,

Thanks for following up with this; we have a ticket reporting the exact same issue/fix in our support queue and will be addressing this in our 3.13 Vybrid kernel support. Though not stated here, is it correct to assume this is while running the Timesys Vybrid kernel?

Thank you,

Timesys Support

0 件の賞賛
返信
7,480件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

markwatson please answer previous question from Timesys

0 件の賞賛
返信
7,480件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you  review this case?

0 件の賞賛
返信
7,480件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport do you have an update?

0 件の賞賛
返信