USB LDO Specification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB LDO Specification

跳至解决方案
8,098 次查看
markwatson
Contributor III

We are seeing some intermittent failures with the USB communication between our device (MVF61NS151...) and a host PC.  I started investigating and noted that the USB Dcap voltage is about 2.7 volts.  The tower board schematic labels this as 3V3 and the VYBRIDFSERIESEC on page 30 shows it as 3p0.  What is the correct voltage for the internal regulator for USB?  My bus voltage is at least 4.9 V, so that is not the problem.  Is there a register setting to disable the internal regulator?  I have no loads on the Dcap piin, just a couple of capacitors.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
7,786 次查看
timesyssupport
Senior Contributor II

Hello Mark,

Thanks for following up with this; we have a ticket reporting the exact same issue/fix in our support queue and will be addressing this in our 3.13 Vybrid kernel support. Though not stated here, is it correct to assume this is while running the Timesys Vybrid kernel?

Thank you,

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
5 回复数
7,786 次查看
markwatson
Contributor III

I have determined that this is intended to be 3.0 V.  The Linux kernel was not enabling the regulator in the ANADIG section in the ANADIG_REG_3P0 register. The lowest order bit must be set. 

0 项奖励
回复
7,787 次查看
timesyssupport
Senior Contributor II

Hello Mark,

Thanks for following up with this; we have a ticket reporting the exact same issue/fix in our support queue and will be addressing this in our 3.13 Vybrid kernel support. Though not stated here, is it correct to assume this is while running the Timesys Vybrid kernel?

Thank you,

Timesys Support

0 项奖励
回复
7,786 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

markwatson please answer previous question from Timesys

0 项奖励
回复
7,786 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you  review this case?

0 项奖励
回复
7,786 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport do you have an update?

0 项奖励
回复