USB Host DMA to internal SRAM - Data abort

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB Host DMA to internal SRAM - Data abort

跳至解决方案
1,666 次查看
ohjana
Contributor I

Hi all,

I use the freescale driver for USB Host to connect a mass storage device and read a file on it into the ddr memory which is attached to the vybrid.

This works well. Now I tried to stream the msd file content to the vybrids internal 512 kByte SRAM. If I do so the vybrid gets an data abort if the DMA

of the host controller starts to stream the msd file content to the internal SRAM.

Picture below shows my intenetion. While the USB Host DMA streams his transaction data into the internal SRAM, the Processor

can do any other stuff on the ddr memory without any interruption.

Why do I get an data abort if the dma starts his work?

Thanks for your help.

0 项奖励
回复
1 解答
1,482 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,483 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
1,483 次查看
timesyssupport
Senior Contributor II

Hello,

Is this issue encountered when running Linux on the Vybrid, or MQX?

Thank you,

Timesys Support

0 项奖励
回复
1,483 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

ohjana​ did you get previous comment?

0 项奖励
回复
1,483 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ are you able to help here?

0 项奖励
回复