Is there a DCU4 driver on the M4 core for MQX?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a DCU4 driver on the M4 core for MQX?

Jump to solution
1,511 Views
markwatson
Contributor III

I have noted the presence of a driver for the DCU4 in the A5 BSP, but not in the M4 BSP.  Is there a driver and/or example code for running the DCU from the M4 core?  Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,375 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
3 Replies
1,376 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,376 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I think the only concern is that MQX for the M4 only executes out of iRAM and to handle pictures you need the DDR which is configured only for the CA5 target.

/Alejandro

0 Kudos
Reply
1,376 Views
rendy
NXP Employee
NXP Employee

Hi, no there isn't such an example, but the DCU driver should work on both cores. You should be able to port the A5 example to M4 core smoothly.

Regards

Rene