TWR-VF65GS10 CTS/RTS connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-VF65GS10 CTS/RTS connection

ソリューションへジャンプ
2,236件の閲覧回数
Hiroki
NXP Employee
NXP Employee

Hi,

TWR-VF65's SCI1 is connected with TWR-SER RS232C port.

However, SCI1_CTS/RTS are not connected with TWR-SER

CTS/RTS. Instead SCI0_CTS/RTS are connected.

Why is TWR-VF65GS10 implemented like that? How can the

user use the flow control on the RS232C of TWR-SER?

Best Regards,

Hiroki

ラベル(1)
0 件の賞賛
返信
1 解決策
2,076件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Hiroki,

  The reason is that the UART1 CTS/RTS signals were being used for other functionality as well as muxed with UART2 which is being used as the secondary UART option, and the main priority for both was basic UART functionality.

  However as a work-around for flow control, you can simply connect B35 to B21 and B39 to A9 on the primary elevator side, which connects UART1 RTCS/CTS to the RTS and CTS pins of the TWR-SER respectively.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,077件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Hiroki,

  The reason is that the UART1 CTS/RTS signals were being used for other functionality as well as muxed with UART2 which is being used as the secondary UART option, and the main priority for both was basic UART functionality.

  However as a work-around for flow control, you can simply connect B35 to B21 and B39 to A9 on the primary elevator side, which connects UART1 RTCS/CTS to the RTS and CTS pins of the TWR-SER respectively.

0 件の賞賛
返信
2,076件の閲覧回数
Hiroki
NXP Employee
NXP Employee

Hi Anthony,

Thank you for your reply.

I understand it.

Hiroki

0 件の賞賛
返信