TWR-VF65GS10 CTS/RTS connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-VF65GS10 CTS/RTS connection

Jump to solution
2,294 Views
Hiroki
NXP Employee
NXP Employee

Hi,

TWR-VF65's SCI1 is connected with TWR-SER RS232C port.

However, SCI1_CTS/RTS are not connected with TWR-SER

CTS/RTS. Instead SCI0_CTS/RTS are connected.

Why is TWR-VF65GS10 implemented like that? How can the

user use the flow control on the RS232C of TWR-SER?

Best Regards,

Hiroki

Labels (1)
0 Kudos
Reply
1 Solution
2,134 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Hiroki,

  The reason is that the UART1 CTS/RTS signals were being used for other functionality as well as muxed with UART2 which is being used as the secondary UART option, and the main priority for both was basic UART functionality.

  However as a work-around for flow control, you can simply connect B35 to B21 and B39 to A9 on the primary elevator side, which connects UART1 RTCS/CTS to the RTS and CTS pins of the TWR-SER respectively.

View solution in original post

0 Kudos
Reply
2 Replies
2,135 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Hiroki,

  The reason is that the UART1 CTS/RTS signals were being used for other functionality as well as muxed with UART2 which is being used as the secondary UART option, and the main priority for both was basic UART functionality.

  However as a work-around for flow control, you can simply connect B35 to B21 and B39 to A9 on the primary elevator side, which connects UART1 RTCS/CTS to the RTS and CTS pins of the TWR-SER respectively.

0 Kudos
Reply
2,134 Views
Hiroki
NXP Employee
NXP Employee

Hi Anthony,

Thank you for your reply.

I understand it.

Hiroki

0 Kudos
Reply