Stop bit of UART for Vybrid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stop bit of UART for Vybrid

Jump to solution
2,060 Views
keisukewatanabe
Contributor III

Dear support,

I want to use the stop bit of UART at 2bit.

I know it is 1bit by default it.

Best regards,

Keisuke Watanabe

Labels (1)
0 Kudos
Reply
1 Solution
1,489 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Keisuke,

  The UART on Vybrid only supports 1 stop bit in normal usage.

  However when ISO-7816 T=0 protocol is used, there is a 2-stop bits feature (see 49.4.8.2 in RM)

-Anthony

View solution in original post

0 Kudos
Reply
3 Replies
1,489 Views
manojunichiro
Contributor I

Hi,

Does it means that it is impossible to set (8,Odd,2) or (8,Even,2) on Vybrid ?

-Junichiro

0 Kudos
Reply
1,490 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Keisuke,

  The UART on Vybrid only supports 1 stop bit in normal usage.

  However when ISO-7816 T=0 protocol is used, there is a 2-stop bits feature (see 49.4.8.2 in RM)

-Anthony

0 Kudos
Reply
1,489 Views
zutter
Contributor II

How many data bits do you need? I create 8,N,2 by 9,N,1 and abuse 9th data bit as stop bit ;-). Similar i did for 7,N,2.

0 Kudos
Reply