SocketCAN performance problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SocketCAN performance problems

ソリューションへジャンプ
21,682件の閲覧回数
kef2
Senior Contributor V

Hello

As everyone CAN'er knows, good old CAN operates at up to 1MHz bit rate clock, one extended ID message is roughly 100 bit times long. That's up to 10k messages per second, which is a piece of cake to handle on 16bit S12 operating at much less than 25MHz bus clock. 10k msgs / sec is also piece of cake for bare metal Vybrid app. But unfortunately it is not a piece of cake for Linux and SocketCAN.

SocketCAN, VF61, 3.13 kernel, no user app working, 5-6 kmsgs / sec on CAN bus. Htop shows ~30% CPU usage... Start one app, which just selects and waits for CAN socket and pulls messages from SocketCAN - CPU usage rises to ~70%... And I would like to have few similar CAN apps operating simultaneously...

Thanks for ideas.

Edward

ラベル(3)
1 解決策
17,931件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
32 返答(返信)
17,932件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
15,538件の閲覧回数
timesyssupport
Senior Contributor II

Hello Edward and karinavalencia​,

We are not able to reproduce the processor consumption on a Tower VF610 evaluation kit.

We have configured and brought up the FlexCAN device, and see .3% CPU consumption at most in Busybox top; running htop, CPU consumption rises to 2%. But we are not seeing any other processor consumption at idle with just the device enabled and configured. Transmitting over CAN also does not show any changes in CPU consumption.

Are you able to provide a test application case which shows this behavior?

Thank you,

Timesys Support

0 件の賞賛
返信
15,538件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

kef2​ can you provide the information requested?

0 件の賞賛
返信
15,534件の閲覧回数
kef2
Senior Contributor V

Hi

Thanks for trying to help solving issue.

Looks like something has changed, perhaps in RFS from my last LinuxLink builds. Previously CPU usage was high like 30% with no CAN app running (kernel only). Starting CAN app (kernel+app) CPU usage was rising to 60% or more depending on message rate. Now with no CAN app running, I see no CPU load, but starting CAN app I see the same 60% for kernel+app. I see high CPU loads only using FlexCAN driver. Using external USB-CAN dongle I see no load, just a couple of % for kernel+app and much higher message rates.

I'll try reproducing issue in new smaller application, also try to figure what's changed that kernel god better and seems not loading alone CPU.

Update1: See attached trycan project. It just waits for can messages using select() and displays message rate. The same problem, high CPU load.

Update2: Well. Finally I found what caused high CPU load with ~6kmsgs/s when CAN app is not running. It was a missing gpio-keys status="disabled" is dts file. (See attached *.dts) Now CPU load is around zero with lots of messages and CAN app (trycan) not running. But question remains, why I see high CPU load when CAN application is running.

Again, what I have.

- untouched kernel image from last LinuxLink build, modified *.dts file as attached.

- ~5800 messages / sec on CAN bus.

- trycan running

- CPU load 40-44%

- htop output:

5871 msgs/s********           44.1%]     Tasks: 8, 0 thr; 2 running
  Mem[*****                  9/120MB]     Load average: 0.37 0.33 0.21
  Swp[#*                       0/0MB]     Uptime: 00:14:47

  PID USER      PRI  NI  VIRT   RES   SHR S CPU% MEM%   TIME+  Command
1178 root       20   0  3016   828   724 S 41.7  0.7  0:11.72 /home/trycan
1179 root       20   0  2884  1180   980 R  1.6  1.0  0:00.80 htop
    1 root       20   0  2276   692   620 S  0.0  0.6  0:00.69 init
1092 root       20   0  2276   448   392 S  0.0  0.4  0:00.00 syslogd
1135 root       20   0  1748   472   396 S  0.0  0.4  0:00.12 /usr/sbin/ifplugd
1151 root       20   0  2228   440   348 S  0.0  0.4  0:00.00 /usr/sbin/dropbea
1159 nobody     20   0  2072   404   268 S  0.0  0.3  0:00.00 /usr/sbin/boa
1167 root       20   0  2280   744   668 S  0.0  0.6  0:00.04 -/bin/sh

Am I doing something silly in my trycan? If so, then why don't I see high CPU load using USB-CAN dongle?

Regards

Edward

0 件の賞賛
返信
15,530件の閲覧回数
timesyssupport
Senior Contributor II

Edward,

The DTS for the the twr-vf610 should note that the GPIO-Keys conflicts with CAN on the i2c bus; this is a comment at ~Line 535.

We will execute your test application and review the results.

Can you clarify what you mean by: ~5800 messages / sec on CAN bus.

What is generating these ~6000 messages? Are those being sent to the hardware - if so, what is sending them?

Thank you,

Timesys Support

0 件の賞賛
返信
15,530件の閲覧回数
kef2
Senior Contributor V

Hi,

Yes, there's a comment at line 535, but no instructions how to disable conflicting button :-). I forgot about it since I was adding functionality and didn't know that CPU gets busy even with no CAN app running. This part of problem is fixed, now CPU is not busy while no CAN app is running.

Some external device is generating those 6k msgs / sec.

Thank you, regards,

Edward

0 件の賞賛
返信
15,530件の閲覧回数
timesyssupport
Senior Contributor II

Hi Edward,

Yes - the comment could be more descriptive. Something along the lines of "To enable CAN, disable GPIO-Keys" would be better.

Thank you - we have a CANbus device we can generate inbound traffic on.

Regards,

Timesys Support

15,530件の閲覧回数
kef2
Senior Contributor V

Hi Timesys Support,

Have you tried reproducing the problem?

Regards,

Edward

0 件の賞賛
返信
15,530件の閲覧回数
kef2
Senior Contributor V

Hi Timesys Support,

any news? Did you try trycan app and can you confirm high CPU usage?

Regards,

Edward

0 件の賞賛
返信
15,530件の閲覧回数
kef2
Senior Contributor V

Hi  timesyssupport   

Hi karinavalencia               

This thread is false "solved", and I even can't change it to "unsolved". FlexCAN driver is still CPU hungry and is much worse than (any?) USB<->CAN dongle. Does anyone at Freescale cars about this? Is "no" - answer to my request? Is this why it is green and answered?

Regards

Edward

0 件の賞賛
返信
15,530件の閲覧回数
timesyssupport
Senior Contributor II

Hi Ed,

Our apologies for the delay in replying; other support interrupts have consumed available cycles to debug this issue.

Our test setup is the TWR-Vybrid VF6 module, with TWR-SER2 module providing CAN interface. We will be testing board to board with i.MX6 SABRE-Lite and, via Kvaser Leaf Light, to generate inbound CAN traffic. Does this match your own hardware setup?

We expect to be able to update whether we are seeing similar traffic tomorrow, 11/19.

Thank you,

Timesys Support

15,530件の閲覧回数
kef2
Senior Contributor V

Hi,

My apologies for not being polite. Yes, TWR-Vybrid VF6 with TWR-SER2, CAN traffic comes to J15 on TWR-SER2. At least confirming the issue would be a great relief.

Thank You,

Edward

0 件の賞賛
返信
15,530件の閲覧回数
timesyssupport
Senior Contributor II

Hello Edward,

We've been working diligently with our Vybrid TWR module to validate the CAN functionality; despite performing the necessary re-work for R10/R11, it seems that we are unable to get any traffic to transmit over the CAN interface on the TWR_SER2 module. We are going to re-work another module and attempt to reproduce. Again, our apologies for the delay.

Thanks,

Timesys Support

15,530件の閲覧回数
kef2
Senior Contributor V

Hello Timesys Support,

Thanks for trying.

1. Please make sure J4 (CAN_ISO) TX and RX jumpers on TWR-SER2 are installed. J4 pins 3-4 and pins 5-6 must be shorted.

2. I remember I had to solder not populated 0 Ohm resistor(s) on TWR-VF65GS10, don't remember which. Please make sure R10 and R11 are soldered.

3. Please don't forget about at least one 120 Ohm termination resistor between CAN_H and CAN_L .

Thanks,

Edward

0 件の賞賛
返信
15,530件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ Please continue with the follow up.

0 件の賞賛
返信
15,537件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help here?

0 件の賞賛
返信
15,537件の閲覧回数
timesyssupport
Senior Contributor II

Hello,

Our testing of CAN has been limited to basic FlexCAN driver functionality in the 3.13 kernel; a loopback on the evaluation board, and between board communication with Vybrid Tower and MX6 based evaluation board. Performance metrics were not captured at this time, but it seems the FlexCAN driver likely needs work to perform well - as evidenced by other instances of the FlexCAN driver on older/current Freescale hardware.

karinavalencia​ - is there a Freescale engineer who may be more familiar with the inner workings of the CAN support to assist?

Thank you,

Timesys Support

15,537件の閲覧回数
kef2
Senior Contributor V

I tried to compare on-chip FlexCAN driver vs sysWORXX USB<->CAN dongle.

1) CAN bus connected to FlexCAN, ~6 kmessages / sec on the bus, CAN application is not running. CPU load is about 30%. Starting CAN application CPU load ~ doubles.

2) CAN bus connected to sysWORXX USB dongle, ~6 kmessages / sec, CAN application running. CPU load << 10%.

No idea how to fix driver. Source looks good.

0 件の賞賛
返信
15,537件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

If you want to increase the performance I would try to use the flexcan driver of MQX with the M4. This in case you need a Real Time feature in your application.

Best Regards,

Alejandro

15,537件の閲覧回数
kef2
Senior Contributor V

Yeah, second MCU or switching to competition MCU also would do. And what to do if VF5's are ordered, no M4 and MQX? Is 6kHz interrupt rate killer for Vybrid Linux? I can't believe that USB is easier to handle with all those layers and etc. Isochronous USB HS still needs 8kHz interrupt rate. Even if interrupt rate is killer, why running read-from-CAN application doubles CPU load? FlexCAN buffers are read already, what's the problem reading buffers from app? Why there's no problem at all doing the same with USB<->CAN dongle?????

0 件の賞賛
返信