SFlash configuration header

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SFlash configuration header

Jump to solution
3,598 Views
tfe
Contributor V

We are working on a custom vybrid-based platform, and are attempting to boot from QSPI1(Spansion S25FL256S). The image we are attempting to boot have been tested and is known to work on the TWR-VF65GS10 kit using QSPI0.

From the Vybrid Manufacturing Tool, we extracted the following header which was contained it a pre-compiled image bundled with the tool.

------------------------- SFLASH CONFIG HEADER START -------------------------

Hold delay: 0 (disabled)

Half Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Half Speed Delay: 0 (One clock cycle delay)

Chip Select hold time: 0

Chip Select setup time: 0

Serial Flash A1 size: 0x01000000 (16MB)

Serial Flash A2 size: 0

Serial Flash B1 size: 0x01000000 (16MB)

Serial Flash B2 size: 0

Serial Clock Frequency: 1 (60 MHz)

Mode of operation of serial Flash: 4 (Quad 4-bit data)

Serial Flash Port B selection: 0 (Port B is not used)

Dual Data Rate mode enable: 0 (DDR mode is disabled)

Data Strobe Signal enable in Serial Flash: 0 (Disable DQS)

Parallel Mode enable: 0 (Disable Parallel Mode in QSPI)

CS1 on Port A: 0 (Disable CS1 on Port A)

CS1 on Port B: 0 (Disable CS1 on Port B)

Full Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Full Speed Delay Selection: 0 (One clock cycle delay)

DDR Sampling Point: 0​

-------------------------- SFLASH CONFIG HEADER END --------------------------

We have attempted to change the "Serial Flash Port B selection" field to 1, set the size of A1 to 0x00 and B1 to 0x02000000, but unfortunately this does not work.

We have set our card to boot from fuses, and set the bootconfig appropriately. Probing the QSPI-flash chip shows that there is traffic between the MCU and chip upon boot.

Does anyone have any input?

Labels (2)
1 Solution
3,322 Views
tfe
Contributor V

I eventually figured this out myself. Only a small modification was necessary:

------------------------- SFLASH CONFIG HEADER START -------------------------

Hold delay: 0 (disabled)

Half Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Half Speed Delay: 0 (One clock cycle delay)

Chip Select hold time: 0

Chip Select setup time: 0

Serial Flash A1 size: 0x02000000 (32MB)

Serial Flash A2 size: 0

Serial Flash B1 size: 0

Serial Flash B2 size: 0

Serial Clock Frequency: 1 (60 MHz)

Mode of operation of serial Flash: 4 (Quad 4-bit data)

Serial Flash Port B selection: 0 (Port B is not used)

Dual Data Rate mode enable: 0 (DDR mode is disabled)

Data Strobe Signal enable in Serial Flash: 0 (Disable DQS)

Parallel Mode enable: 0 (Disable Parallel Mode in QSPI)

CS1 on Port A: 0 (Disable CS1 on Port A)

CS1 on Port B: 0 (Disable CS1 on Port B)

Full Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Full Speed Delay Selection: 0 (One clock cycle delay)

DDR Sampling Point: 0

-------------------------- SFLASH CONFIG HEADER END --------------------------

Cheers

View solution in original post

0 Kudos
Reply
4 Replies
3,323 Views
tfe
Contributor V

I eventually figured this out myself. Only a small modification was necessary:

------------------------- SFLASH CONFIG HEADER START -------------------------

Hold delay: 0 (disabled)

Half Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Half Speed Delay: 0 (One clock cycle delay)

Chip Select hold time: 0

Chip Select setup time: 0

Serial Flash A1 size: 0x02000000 (32MB)

Serial Flash A2 size: 0

Serial Flash B1 size: 0

Serial Flash B2 size: 0

Serial Clock Frequency: 1 (60 MHz)

Mode of operation of serial Flash: 4 (Quad 4-bit data)

Serial Flash Port B selection: 0 (Port B is not used)

Dual Data Rate mode enable: 0 (DDR mode is disabled)

Data Strobe Signal enable in Serial Flash: 0 (Disable DQS)

Parallel Mode enable: 0 (Disable Parallel Mode in QSPI)

CS1 on Port A: 0 (Disable CS1 on Port A)

CS1 on Port B: 0 (Disable CS1 on Port B)

Full Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Full Speed Delay Selection: 0 (One clock cycle delay)

DDR Sampling Point: 0

-------------------------- SFLASH CONFIG HEADER END --------------------------

Cheers

0 Kudos
Reply
3,322 Views
timesyssupport
Senior Contributor II

Hello,

We are currently looking into this, and attempting to determine a cause. We will follow up when we have some insight.

Thank you,

Timesys Support

3,322 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ do you have an update?

0 Kudos
Reply
3,322 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ are you able  to  attend this case?

0 Kudos
Reply