hi,I use the simple DMA mode of the SDHC' internal DMA with Vybrid Tower.The OS is MQX 4.0.2.When I select "DDR debug" with IAR,the file in the SD card was not written or readed correctly.But,when I select "Int Ram debug",the file was written or readed correctly.On the datasheet <vybrid Reference manual> page 2742,it say "the SDHC internal DMA does support a virtual memory system".I want to know ,how to use simple DMA in DDR mode with Vybrid Tower system?