Reference Manual rev 4, Missing SNVS RTC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reference Manual rev 4, Missing SNVS RTC

Jump to solution
2,700 Views
snowholgi
Contributor I

Hello after taking a look in the revision history of the new reference manual rev 4, I see that SNVS documentation is removd from the manual.

Does this mean, that there is no RTC in the device ?

Hope this is not true

Holger

0 Kudos
Reply
1 Solution
2,476 Views
RossMcLuckie
NXP Employee
NXP Employee

Correct, RTC is available on parts without security.

View solution in original post

0 Kudos
Reply
4 Replies
2,476 Views
RossMcLuckie
NXP Employee
NXP Employee

RTC is still there, this is just a temporary thing. For this release we are splitting out the security related material into a separate Security Reference Manual. The SNVS chapter has a lot of security related material, but also some general content, including the RTC which will be put back into the standard Reference Manual on the next release, we were not able to complete the separation work on time for this release, an addendum will follow shortly.

0 Kudos
Reply
2,476 Views
hmijail
Contributor II

One year and 3 revisions later, the Vybrid Reference Manual still contains no information about the RTC.

Maybe I am missing something, but I can't be sure because the revision history seems to have disappeared from the Reference Manual.

Any plans about improving the situation?

0 Kudos
Reply
2,476 Views
snowholgi
Contributor I

Thank a lot for this information.

So I can assume, that RTC is in the device also in case we haven't ordered the security features.

Right ?

0 Kudos
Reply
2,477 Views
RossMcLuckie
NXP Employee
NXP Employee

Correct, RTC is available on parts without security.

0 Kudos
Reply