Reference Manual rev 4, Missing SNVS RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reference Manual rev 4, Missing SNVS RTC

ソリューションへジャンプ
2,761件の閲覧回数
snowholgi
Contributor I

Hello after taking a look in the revision history of the new reference manual rev 4, I see that SNVS documentation is removd from the manual.

Does this mean, that there is no RTC in the device ?

Hope this is not true

Holger

0 件の賞賛
返信
1 解決策
2,537件の閲覧回数
RossMcLuckie
NXP Employee
NXP Employee

Correct, RTC is available on parts without security.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,537件の閲覧回数
RossMcLuckie
NXP Employee
NXP Employee

RTC is still there, this is just a temporary thing. For this release we are splitting out the security related material into a separate Security Reference Manual. The SNVS chapter has a lot of security related material, but also some general content, including the RTC which will be put back into the standard Reference Manual on the next release, we were not able to complete the separation work on time for this release, an addendum will follow shortly.

0 件の賞賛
返信
2,537件の閲覧回数
hmijail
Contributor II

One year and 3 revisions later, the Vybrid Reference Manual still contains no information about the RTC.

Maybe I am missing something, but I can't be sure because the revision history seems to have disappeared from the Reference Manual.

Any plans about improving the situation?

0 件の賞賛
返信
2,537件の閲覧回数
snowholgi
Contributor I

Thank a lot for this information.

So I can assume, that RTC is in the device also in case we haven't ordered the security features.

Right ?

0 件の賞賛
返信
2,538件の閲覧回数
RossMcLuckie
NXP Employee
NXP Employee

Correct, RTC is available on parts without security.

0 件の賞賛
返信