Reference Manual rev 4, Missing SNVS RTC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Reference Manual rev 4, Missing SNVS RTC

跳至解决方案
1,918 次查看
snowholgi
Contributor I

Hello after taking a look in the revision history of the new reference manual rev 4, I see that SNVS documentation is removd from the manual.

Does this mean, that there is no RTC in the device ?

Hope this is not true

Holger

0 项奖励
回复
1 解答
1,694 次查看
RossMcLuckie
NXP Employee
NXP Employee

Correct, RTC is available on parts without security.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,694 次查看
RossMcLuckie
NXP Employee
NXP Employee

RTC is still there, this is just a temporary thing. For this release we are splitting out the security related material into a separate Security Reference Manual. The SNVS chapter has a lot of security related material, but also some general content, including the RTC which will be put back into the standard Reference Manual on the next release, we were not able to complete the separation work on time for this release, an addendum will follow shortly.

0 项奖励
回复
1,694 次查看
hmijail
Contributor II

One year and 3 revisions later, the Vybrid Reference Manual still contains no information about the RTC.

Maybe I am missing something, but I can't be sure because the revision history seems to have disappeared from the Reference Manual.

Any plans about improving the situation?

0 项奖励
回复
1,694 次查看
snowholgi
Contributor I

Thank a lot for this information.

So I can assume, that RTC is in the device also in case we haven't ordered the security features.

Right ?

0 项奖励
回复
1,695 次查看
RossMcLuckie
NXP Employee
NXP Employee

Correct, RTC is available on parts without security.

0 项奖励
回复