Question WDOG_WCR Manual Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question WDOG_WCR Manual Issue

2,315 Views
soichiyamamoto
Contributor V

Hi,


I ask about  manual issue.


The bit array of a figure is different from a bit array of a table in 26.6.1 Watchdog Control Register (WDOG_WCR)/WDOG_WCR field descriptions .(VYBRIDRM.pdf/1136page )


Is bit array of a table right?

Best Regards,

soichi

Labels (1)
0 Kudos
Reply
5 Replies

2,039 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

May you clarify, please, what specific difference you are asking about?

Thanks, Naoum Gitnik.

0 Kudos
Reply

2,039 Views
soichiyamamoto
Contributor V

Dear Naoum,


Thank you for reply.


A difference between figure and table is as follows


a figure

  15-8 : WT

     7 : SRE

     6 : WDA

     5 : SRS

     4 : WDE

     3 : WDBG

     2 : WDZST

a table:

 15-8 : WT

     6 : SRE

     5 : WDA

     4 : SRS

     2 : WDE

     1 : WDBG

     0 : WDZST

Best regards,

soichi

a figure:

wd1.png

a table:

wd2.png


0 Kudos
Reply

2,039 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

Sorry for taking that long to answer it, but I got clarification that the the bit mapping in the table is correct.

I will request the documentation correction.

Thanks for catching it!

Regards, Naoum Gitnik.

0 Kudos
Reply

2,039 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

Any success so far with our published code, please?

Regards, Naoum Gitnik.

0 Kudos
Reply

2,039 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

It looks to me like a typo.

Before starting checking it with the design team, may I ask you if you verified the bits use/descriptions in our published code? - This code is tested and quite well commented, therefore it is a trusted source of information.

Thanks, Naoum Gitnik.

0 Kudos
Reply