Processor With Device Level Ring(DLR) support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor With Device Level Ring(DLR) support

2,093 Views
praveenb
Contributor I

I need list for processor which supports Device Level Ring(DLR) in Ethernet -inbuilt switch. i saw this two part numbers VF5XX &VF6XX it has L2 Switch but i am not sure its supports DLR. please clarify these two will support DLR or not, and also suggest few other processor with DLR support

Note: no plan to add a external switch for DLR

 

Thanks & Regards

Praveen B

0 Kudos
Reply
1 Reply

1,857 Views
art
NXP Employee
NXP Employee

The VF5XX & VF6XX controllers don't have any built-in feature for direct DLR protocol support. The support for this protocol should be implemented in software, if required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply