Processor With Device Level Ring(DLR) support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor With Device Level Ring(DLR) support

2,096件の閲覧回数
praveenb
Contributor I

I need list for processor which supports Device Level Ring(DLR) in Ethernet -inbuilt switch. i saw this two part numbers VF5XX &VF6XX it has L2 Switch but i am not sure its supports DLR. please clarify these two will support DLR or not, and also suggest few other processor with DLR support

Note: no plan to add a external switch for DLR

 

Thanks & Regards

Praveen B

0 件の賞賛
返信
1 返信

1,860件の閲覧回数
art
NXP Employee
NXP Employee

The VF5XX & VF6XX controllers don't have any built-in feature for direct DLR protocol support. The support for this protocol should be implemented in software, if required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信