Not able to get RESET_OUT# signal in software reboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to get RESET_OUT# signal in software reboot

1,006件の閲覧回数
drashtiparikh
Contributor I

Hello,


I am working on VF61 module and collibri evaluation board V3.2A.
I have observed that when there is a hard reboot I get reset RESET_OUT# signal through X3 -> B32 pin of collibri evaluation board, but when i do software reset/reboot I am not able to get that signal.
Is this an expected behaviour?
I think software reboot should also give RESET_OUT# signal. Are there any necessary steps to follow to get RESET_OUT# signal in software reboot as well?

Please let me know if any further information is required.

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

815件の閲覧回数
art
NXP Employee
NXP Employee

Q. Is this an expected behaviour?

A. Yes, this is the expected behaviour. The RESET_OUT# signal is not asserted during the software reboot.

Q. Are there any necessary steps to follow to get RESET_OUT# signal in software reboot as well?

A. There is no way to assert the RESET_OUT# signal during the software reboot.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信