NAND Boot with Linux 3.13

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Boot with Linux 3.13

2,700件の閲覧回数
Nouchi
Senior Contributor II

Hello,

I'm beginning to play with Linux-3.13 and u-boot-2013.07 on tower board, and I'm looking for a good "Howto" to configure the system booting on NAND flash.

I've few questions :

- Where and how to write device tree block on flash?

- How partitioning NAND flash, the old way don't work any more? ( mtdparts=NAND:  etc.....)

- From timesys factory, how to rebuild the device tree?

Best regards,

Emmanuel


ラベル(4)
0 件の賞賛
返信
5 返答(返信)

2,422件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I am sure Timesys will provide more information in regards their BSP I just wonder if you have checked this :

https://linuxlink.timesys.com/docs/projects/engineering/wiki/NAND_Boot_for_Vybrid_Tower

Best Regards,

Alejandro

0 件の賞賛
返信

2,422件の閲覧回数
Nouchi
Senior Contributor II
0 件の賞賛
返信

2,422件の閲覧回数
timesyssupport
Senior Contributor II

Hello,

Thank you for following up - yes, we are in the process of updating the Vybrid documentation to reflect changes for the 3.13 release.

The HOWTO Ubifs document is somewhat general; typically we suggest reviewing the MTD documentation located here for management of UBIFS rootfs:

http://www.linux-mtd.infradead.org/doc/ubifs.html

The Vybrid-specific information we will review and update. We will follow up in this thread once the process has been documented.

Thanks,

Timesys Support

2,422件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport do you have an update?

0 件の賞賛
返信

2,422件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help to check this case?

0 件の賞賛
返信