Motor Control using M4 in Vybrid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Motor Control using M4 in Vybrid

跳至解决方案
2,650 次查看
afzalmohammed
Contributor I

Hi,

Are there any software support available for motor control using Vybrid Cortex M4, seems there is motor control support in Kinetics V series (that have Cortex M4), can it be used with Vybrid M4 too?

Regards

afzal

标签 (1)
0 项奖励
回复
1 解答
2,508 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,509 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
2,511 次查看
rendy
NXP Employee
NXP Employee

Hello,

There is no special support for this. I don't know much about Kinetises or about motor control but if there are peripherals on Vybrid which you need for motor control (PWMs?) and if you have some motor control code for another Cortex M4, then it's very likely that you can port the code to Vybrid easily.

Regards

Rene

0 项奖励
回复