Motor Control using M4 in Vybrid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Motor Control using M4 in Vybrid

Jump to solution
2,627 Views
afzalmohammed
Contributor I

Hi,

Are there any software support available for motor control using Vybrid Cortex M4, seems there is motor control support in Kinetics V series (that have Cortex M4), can it be used with Vybrid M4 too?

Regards

afzal

Labels (1)
0 Kudos
Reply
1 Solution
2,485 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
2,486 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,488 Views
rendy
NXP Employee
NXP Employee

Hello,

There is no special support for this. I don't know much about Kinetises or about motor control but if there are peripherals on Vybrid which you need for motor control (PWMs?) and if you have some motor control code for another Cortex M4, then it's very likely that you can port the code to Vybrid easily.

Regards

Rene

0 Kudos
Reply