MfgTool issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,200件の閲覧回数
mplseng
Contributor II

When I try to use a version of u-boot built using the latest git sources, I get the error  "ModuleID[2] LevelID[1]: Failed to read HAB type from ROM!!! ".

Any suggestion as to how I can resolve this?

Bob

ラベル(1)
1 解決策
2,625件の閲覧回数
mplseng
Contributor II

The downloader requires a "version 3" header. The open source version of u-boot does not support this header type. We added the type which affected imximage.cfg, tools/imximage.c, and tools/imximage.h. This resolved the "HAB" error.

元の投稿で解決策を見る

3 返答(返信)
2,626件の閲覧回数
mplseng
Contributor II

The downloader requires a "version 3" header. The open source version of u-boot does not support this header type. We added the type which affected imximage.cfg, tools/imximage.c, and tools/imximage.h. This resolved the "HAB" error.

2,625件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

Are you using MfgTool to flash this u-boot on SD, NAND, QSPI??

When do you see those messages, when flashing, when trying to boot?

Can you share the u-boot binary you are trying to flash to try it at my end?

0 件の賞賛
返信
2,623件の閲覧回数
mplseng
Contributor II

I am using the manufacturing tool to flash my build of u-boot to SD.

Attached

0 件の賞賛
返信