MVF61NN151CMK10/NAND flash memory and SPI flash memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MVF61NN151CMK10/NAND flash memory and SPI flash memory

1,956 次查看
soichiyamamoto
Contributor V

Hello

I use MVF61NN151CMK10.

NAND flash memory and SPI flash memory wants to uses  MT29F4G08ABADAWP-IT:D and M25P128-VMF6TPB.

I think that will be no problem with this method.

Is this all right?

Please give me comment.

Best Regards,

soichi yamamoto

0 项奖励
回复
3 回复数

1,769 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

ioseph_martinez can you review this case and provide follow up?

0 项奖励
回复

1,769 次查看
soichiyamamoto
Contributor V

Hi Karina Valencia Aguilar,

Thank you very much.

Yes

Best Regards,

soichi yamamoto

0 项奖励
回复

1,769 次查看
ioseph_martinez
NXP Employee
NXP Employee

Hi Soichi-san,

I have access to the SPI NOR memory but not the NAND memory datasheet.

I checked SPI NOR memory datasheet seems fine. I expect is possible to use this device but you would need to do some testing to confirm this 100%

Regarding the NAND memory I cannot comment since I don't have access to that memory.

Which device do you plan to use for system boot, the NAND or the SPI-NOR?

Best Regards,

Ioseph

0 项奖励
回复