Hello Folks;
I want to use SysRAM0 + SysRam1 for Code and GfxRAM for Data
Is it posbile ?
I have changed scatter file and It does not work.
I can't figure out why ?
And one more thing, Is it posible to use SysRAM0 for both code and data ?
Thank you for everything.
#! armcc -E --cpu Cortex-A5.neon
#define CODE_BASE_ADDR_START 0x3f000000
#define CODE_BASE_ADDR_END 0x3f070000
#define CODE_SIZE (CODE_BASE_ADDR_END - CODE_BASE_ADDR_START)
#define DATA_BASE_ADDR_START 0x3f410000
#define DATA_BASE_ADDR_END 0x3f470000
#define DATA_SIZE (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START)
#define DATA_SHARED_START 0x3f400000
#define DATA_SHARED_END 0x3f40fff0
#define BOOT_STACK_SIZE 0x100
#define FIQ_STACK_SIZE 0
#define ABT_STACK_SIZE 0
#define UND_STACK_SIZE 0
#define SYS_STACK_SIZE 0
LOAD_REGION_CODE CODE_BASE_ADDR_START
{
BOOT +0
{
*(STARTUP)
}
CODE +0
{
* (InRoot$$Sections) ; All library sections for example, __main.o,
; __scatter*.o, __dc*.o, and * Region$$Table
* (KERNEL)
* (TEXT)
* (+RO)
}
DATA DATA_BASE_ADDR_START ALIGN 32
{
* (+RW, +ZI)
}
; FIQ stack
FIQ_STACKS +0 ALIGN 8 EMPTY FIQ_STACK_SIZE {}
; ABT stack
ABT_STACKS +0 ALIGN 8 EMPTY ABT_STACK_SIZE {}
; UND stack
UND_STACKS +0 ALIGN 8 EMPTY UND_STACK_SIZE {}
; SYS stack
SYS_STACKS +0 ALIGN 8 EMPTY SYS_STACK_SIZE {}
KERNEL_DATA_START +0 ALIGN 16
{
* (KERNEL_DATA_START) ; start of kernel data
* (SRAM_POOL_START)
* (UNCACHED_DATA_START)
}
KERNEL_DATA_END DATA_BASE_ADDR_END - (0x03*0x10) ; RAM_END - 3 x aligned value with align 0x04
{
* (SRAM_POOL_END)
* (UNCACHED_DATA_END)
* (KERNEL_DATA_END) ; end of kernel data
}
SHARED_RAM_START DATA_SHARED_START EMPTY 0xfff0
{
}
SHARED_RAM_END DATA_SHARED_END
{
*(SHARED_RAM_END)
}
; mem_init writes a storeblock_struct at the end of kernel data,
; max size 32 bytes, so use 0x100 offset
BOOT_STACK_ADDR (DATA_BASE_ADDR_END - BOOT_STACK_SIZE) OVERLAY
{
*(BOOT_STACK)
}
; We don't use their stack or heap, but the tools expect this
; to be here, so we have a dummy placeholder.
ARM_LIB_STACKHEAP (DATA_BASE_ADDR_END - 0x100) OVERLAY EMPTY UNINIT 0x04
{
}
}
Hello,
I have tried using SysRAM0 for code and GfxRAM for data, and SysRAM0 for both code and data successfully. I tested with the "pingpong" example MCC application on the M4 core. In the first case, I specified 0x3f000000-0x3f02fff0 for code, and 0x3f400000-0x3f407ff0 for data; in the second case, I specified 0x3f000000-0x3f02fff0 for code, and 0x3f030000-0x3f037ff0 for data.
When you modified the scatter file - did you change the scatter file at FreescaleMQXRTOS4.0.2-GA/mqx/source/bsp/...? This is what I did, then cleaned all MQX projects (bsp, psp, application) and rebuilt.
Thanks,
Timesys Support
Is it possible to use gfxRAM to execute M4/MQX code?
Hi Jack,
I did not get a chance to try this today. I will try Monday and let you know how it goes.
Thanks,
Timesys Support
Hello Jack,
I was not able to fully run an MQX application in gfxram. IE, configuring the scatter file in this fashion did not work:
| #define CODE_BASE_ADDR_START | 0x3f400000 |
| #define CODE_BASE_ADDR_END | 0x3f43fff0 |
| #define CODE_SIZE | (CODE_BASE_ADDR_END - CODE_BASE_ADDR_START) |
| #define DATA_BASE_ADDR_START | 0x3f450000 |
| #define DATA_BASE_ADDR_END | 0x3f457ff0 |
| #define DATA_SIZE | (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START) |
| #define DATA_SHARED_START | 0x3f440000 |
| #define DATA_SHARED_END | 0x3f44fff0 |
In order for the program to run, I needed to change DATA_SHARED_START and DATA_SHARED_END to be located in OCRAM.
Thanks, and let me know if you have any questions.
Timesys Support
timesyssupport can you attend this case?