MQX Scatter Loading and GfxRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX Scatter Loading and GfxRAM

3,459 Views
ngsari
Contributor II

Hello Folks;

I want to use SysRAM0 + SysRam1 for Code and GfxRAM for Data

Is it posbile ?

I have changed scatter file and It does not work.
I can't figure out why ?

And one more thing, Is it posible to use SysRAM0 for both code and data ?

Thank you for everything.

#! armcc -E --cpu Cortex-A5.neon

#define CODE_BASE_ADDR_START    0x3f000000

#define CODE_BASE_ADDR_END      0x3f070000

#define CODE_SIZE               (CODE_BASE_ADDR_END - CODE_BASE_ADDR_START)

#define DATA_BASE_ADDR_START    0x3f410000

#define DATA_BASE_ADDR_END      0x3f470000

#define DATA_SIZE               (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START)

#define DATA_SHARED_START       0x3f400000

#define DATA_SHARED_END         0x3f40fff0

#define BOOT_STACK_SIZE         0x100

#define FIQ_STACK_SIZE          0

#define ABT_STACK_SIZE          0

#define UND_STACK_SIZE          0

#define SYS_STACK_SIZE          0

LOAD_REGION_CODE CODE_BASE_ADDR_START

{

    BOOT +0

    {

        *(STARTUP)

    }

   

    CODE +0

    {

        * (InRoot$$Sections)      ; All library sections for example, __main.o,

                                  ; __scatter*.o, __dc*.o, and * Region$$Table

        * (KERNEL)

        * (TEXT)

        * (+RO)

    }

   

    DATA DATA_BASE_ADDR_START ALIGN 32

    {

        * (+RW, +ZI)

    }

    ; FIQ stack

    FIQ_STACKS +0 ALIGN 8 EMPTY FIQ_STACK_SIZE {}

    ; ABT stack

    ABT_STACKS +0 ALIGN 8 EMPTY ABT_STACK_SIZE {}

    ; UND stack

    UND_STACKS +0 ALIGN 8 EMPTY UND_STACK_SIZE {}

    ; SYS stack

    SYS_STACKS +0 ALIGN 8 EMPTY SYS_STACK_SIZE {}

    KERNEL_DATA_START +0 ALIGN 16

    {

        * (KERNEL_DATA_START)     ; start of kernel data

        * (SRAM_POOL_START)

        * (UNCACHED_DATA_START)

    }

    KERNEL_DATA_END DATA_BASE_ADDR_END - (0x03*0x10)      ; RAM_END - 3 x aligned value with align 0x04

    {

        * (SRAM_POOL_END)

        * (UNCACHED_DATA_END)

        * (KERNEL_DATA_END)     ; end of kernel data

    }

    SHARED_RAM_START DATA_SHARED_START EMPTY 0xfff0

    {

    }

    SHARED_RAM_END DATA_SHARED_END

    {

        *(SHARED_RAM_END)

    }

   

    ; mem_init writes a storeblock_struct at the end of kernel data,

    ; max size 32 bytes, so use 0x100 offset

  

    BOOT_STACK_ADDR (DATA_BASE_ADDR_END - BOOT_STACK_SIZE) OVERLAY

    {

        *(BOOT_STACK)

    }

    ; We don't use their stack or heap, but the tools expect this

    ; to be here, so we have a dummy placeholder.

    ARM_LIB_STACKHEAP (DATA_BASE_ADDR_END - 0x100) OVERLAY EMPTY UNINIT 0x04

    {

    }

   

}

Labels (2)
6 Replies

2,973 Views
timesyssupport
Senior Contributor II

Hello,

I have tried using SysRAM0 for code and GfxRAM for data, and SysRAM0 for both code and data successfully. I tested with the "pingpong" example MCC application on the M4 core. In the first case, I specified 0x3f000000-0x3f02fff0 for code, and 0x3f400000-0x3f407ff0 for data; in the second case, I specified 0x3f000000-0x3f02fff0 for code, and 0x3f030000-0x3f037ff0 for data.


When you modified the scatter file - did you change the scatter file at FreescaleMQXRTOS4.0.2-GA/mqx/source/bsp/...? This is what I did, then cleaned all MQX projects (bsp, psp, application) and rebuilt.


Thanks,


Timesys Support

2,973 Views
jackblather
Senior Contributor I

Is it possible to use gfxRAM to execute M4/MQX code?

0 Kudos
Reply

2,973 Views
timesyssupport
Senior Contributor II

Hi Jack,


I did not get a chance to try this today. I will try Monday and let you know how it goes.

Thanks,

Timesys Support

0 Kudos
Reply

2,973 Views
jackblather
Senior Contributor I

Thanks so much.

0 Kudos
Reply

2,973 Views
timesyssupport
Senior Contributor II

Hello Jack,

I was not able to fully run an MQX application in gfxram. IE, configuring the scatter file in this fashion did not work:

#define CODE_BASE_ADDR_START0x3f400000
#define CODE_BASE_ADDR_END  0x3f43fff0
#define CODE_SIZE           (CODE_BASE_ADDR_END - CODE_BASE_ADDR_START)

#define DATA_BASE_ADDR_START0x3f450000
#define DATA_BASE_ADDR_END  0x3f457ff0
#define DATA_SIZE           (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START)

#define DATA_SHARED_START   0x3f440000
#define DATA_SHARED_END     0x3f44fff0

In order for the program to run, I needed to change DATA_SHARED_START and DATA_SHARED_END to be located in OCRAM.

Thanks, and let me know if you have any questions.

Timesys Support

2,973 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you  attend this case?

0 Kudos
Reply