MQX Interrupt Shared Peripheral Routing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX Interrupt Shared Peripheral Routing

4,648 Views
carlovalgocela
Contributor III

Reading the Vybrid AN4947.pdf,  and in 4.2 Dual-core communication and synchronization options,

• Interrupts. Routing options for both cores — none, one, or both cores can be notified for the event.

I wanted for  M4 MQX NVIC Interrupt 10 and 11 not to be shared on the A5 Linux.

I use this code to configure the routing.

/* Disable shared interrupt to A5 Core */

    _irouter_routing(26,0,0);

    _irouter_routing(27,0,0);

However it is not working. A5 Linux could still received and processed the interrupts.

Any ideas what I missed?

interrupt.png

I'm using MQX Version 4.1.1

Thanks,

Carlo Val

Labels (3)
0 Kudos
Reply
7 Replies

4,293 Views
karina_valencia
NXP Apps Support
NXP Apps Support

alejandrolozano​ are you able to help here?

0 Kudos
Reply

4,291 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I'd like to reproduce the behavior first. Carlo, which Linux BSP are you using?

Best Regards,

Alejandro

0 Kudos
Reply

4,291 Views
carlovalgocela
Contributor III

I'm using Linux version 3.0.15-ts-armv7l .

I saw yesterday in a file init_gic.c  routing all interrupts to Core 1.

Ill try it today and see if it will work

Here is my update would be:

volatile uint16_t *ptr26;

volatile uint16_t *ptr27;

ptr26 = &MSCM_IRSPRC26;

*ptr26 = MSCM_IRSPRC_CP1En_MASK; /* route interrupts to core 1*/

ptr27 = &MSCM_IRSPRC27;

*ptr27 = MSCM_IRSPRC_CP1En_MASK; /* route interrupts to core 1*/

0 Kudos
Reply

4,291 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Carlo,

Did you modification work?

Regards,

Alejandro

0 Kudos
Reply

4,291 Views
carlovalgocela
Contributor III

Hello alejandrolozano​,

No it didn't work :-(

0 Kudos
Reply

4,291 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

On Linux side you could try to disable the interrupt routed to the A5 corresponding to the DMA.

void mvf_init_irq(void)

{

        unsigned int i;

        void __iomem *int_router_base =

                                MVF_IO_ADDRESS(MVF_MSCM_INT_ROUTER_BASE);

        struct irq_desc *desc;

        unsigned short route;

        /* start offset if private timer irq id, which is 29.

         * ID table:

         * Global timer, PPI -> ID27

         * A legacy nFIQ, PPI -> ID28

         * Private timer, PPI -> ID29

         * Watchdog timers, PPI -> ID30

         * A legacy nIRQ, PPI -> ID31

         */

        gic_init(0, 27, MVF_IO_ADDRESS(MVF_INTD_BASE_ADDR),

                MVF_IO_ADDRESS(MVF_SCUGIC_BASE_ADDR + 0x100));

        for (i = MXC_INT_START; i <= MXC_INT_END; i++) {

                desc = irq_to_desc(i);

                desc->irq_data.chip->irq_set_wake = mvf_gic_irq_set_wake;

        }

        mvf_register_gpios();

        int_router_base += 0x80;

        for (i = 0; i < 112; i++) {

                route = 1 | __raw_readw(int_router_base);

                __raw_writew(route, int_router_base);

                int_router_base += 2;

        }

}

This function is found at vim arch/arm/mach-mvf/irq.c

Let me debug the M4 (MQX side) to verify the possible problem.

Best Regards,

Alejandro

4,291 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Carlo,

Did you try the previous suggestion?

Best Regards,

Alejandro

0 Kudos
Reply