Hello JBS,
I believe you can run M4 from DDR, but the problem will be the possible wait states as you will be charing the DDR bus with both processors and other peripherals.
Usually, customers need to guarantee the M4 application will be real time and deterministic; and having the possibility of not having the bus ready at any time might be an issue on those cases.
Anyway, if you want to test that, I would suggest you to run instructions like these from uboot or linux:
(Please notice these are only examples, and you will need to change the addresses, they most probably are pointing to internal SRAM).
From uboot:
setenv bootcmd 'fatload mmc 0:1 0x81000000 uImage-3.0-ts-armv7l;fatload mmc 0:1 0x3f000000 oobe_twrvf65gs10_m4.bin;mw.l 0x4006e028 0x3f000485;mw.l 0x4006b08c 0x00015a5a;bootm 0x81000000'
From Linux:
modprobe mcc
mqxboot pingpong_example_twrvf65gs10_m4.bin 0x3f000000 0x3f000485
Other possibilities are:
Having an SRAM connected on the Flexbus and running from there.
The QSPI should be also compatible with QSPI DDR RAMs, instead of Flash (not sure if it helps anything).
BR,
Bruno