Dear NC PUTHUFF,
Sorry, I missed the point that the thread was private but it looks like the information in it is actually not.
-----------------------------------------------
I could enable tracing with DS-5 without replacing damping resistors so far.
The reason why I failed to enable it was that I used Ethernet to connect DSTREAM. DSTREAM should be connected through USB to enable tracing.
...
So the 1st step that confirming tracing with DS-5 was resolved.
However the customer still has problems that some TPIU registers couldn't be accessed. In my environment, I couldn't access these registers.
Can you access them?
Could you, please, give me some advices for this?
...
Tracing is now working on the customer side by enabling trace interface IOMUX.
Regarding TPIU register access failure I asked you, this was because customer sent me wrong base address for TPIU. now we can access TPIU registers. All issues are closed. Thank you for your time.
...
For Vybrid part, no more register setting is required.
However some configuration on debugger software would be needed.
In case of DS-5 + DSTREAM, you may need DTSL (Debug and Trace Service Layer) configuration.
In my experience, "Trace capture method" should be "On Chip Trace Buffer (ETB)", then it works.
...
In addition, I have only tried tracing BootROM contents, not for software project.
So, only executed the .ds script file (attached), then run processor or execute instruction by step.
-----------------------------------------------------------
Hopefully it helps.
Regards, Naoum Gitnik.