In the dual core VF6 can I only boot the m4 core to minimize system power in certain applications?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

In the dual core VF6 can I only boot the m4 core to minimize system power in certain applications?

2,676 次查看
kenmcdaniel
Contributor I

Few questions on the VF6xx cores:


Can I only boot the m4 core (keeping the A5 off or stopped) in the VF6xx  to minimize system power in certain applications?

Will the m4 core have access to the nand and ddr controllers if the A5 core is off?

What are typical power measurement in low power modes if the m4 is running and the A5 core is off/stopped?

Thanks,

Ken

标签 (1)
0 项奖励
回复
12 回复数

2,280 次查看
alejandrolozan1
NXP Employee
NXP Employee

From the below thread:

Hi, the answer depends on which core is the primary one. If A5 is the primary core, then you could you could put the core into one of the three LPStop modes. If A5 is the

secondary core, you can disable it with writing '0x5A5A' into CCM_CCOWR register.

Re: Re: Need a code sequence to shutdown the Cortex A5 core

Best Regards,

Alejandro

2,280 次查看
swapnilv
Contributor III

Hi,

I am not able to access the link mentioned by you

Re: Re: Need a code sequence to shutdown the Cortex A5 core

https://community.freescale.com/message/423803#423803

I get below message when I try to access the link.

"Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here."

0 项奖励
回复

2,280 次查看
alejandrolozan1
NXP Employee
NXP Employee

Sorry, what it matters is that if A5 is the primary core, then you could you could put the core into one of the three LPStop modes. If A5 is the secondary core, you can disable it with writing '0x5A5A' into CCM_CCOWR register.

Best Regards,

Alejandro

2,280 次查看
swapnilv
Contributor III

Hi,

Any updates for the questions that I have asked previously regarding disabling primary A5 Core and how to put it in LPstop mode?

Thanks in advance..

Swapnil

0 项奖励
回复

2,280 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

You can find code that explains in detail how to change from one power mode to another in the baremetal sample code:

Sample Code for Vybrid Controller Tower System

I think you may find it very useful.

Best Regards,

Alejandro

2,280 次查看
kenmcdaniel
Contributor I

Hi,

We have the dual core A5/M4 Vybrid Controller Tower System and the sample code does not put the A5 in LPSTOP. Is there a problem with the sample code?

-ken

0 项奖励
回复

2,280 次查看
alejandrolozan1
NXP Employee
NXP Employee

The LPSTOP mode will enter until both cores execute the "wfi" instruction. If CA5 executes the wfi, this will halt  but the entire system (SoC) will not mode to LPSTOP mode. 

/Alejandro

2,280 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

alejandrolozano please continue with the follow up.

0 项奖励
回复

2,280 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

alejandrolozano​ any  update?

0 项奖励
回复

2,280 次查看
swapnilv
Contributor III

Thanks for your reply..

I am using pcm052 PhyCORE-Vybrid development kit which has A5 as primary core.

What I want to do is disable A5 core completely and only run MQX applications on M4 core.

So my question is:

1. Does "Putting A5 into LPstop mode" means there is a software mechanism for this and A5 will be completely disabled and I will be able to boot the board with M4 core only?

2. Could you please guide me how I can put A5 into  LPstop mode?

3. Do I need to make any changes in uboot bootloader if I wish to disable A5 core and boot directly from M4 core MQX application?

Thanks in advance,

Swapnil

0 项奖励
回复

2,280 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

alejandrolozano​ please check it

0 项奖励
回复

2,280 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help here?

0 项奖励
回复