In Vybrid F-Series, is the clock frequency of 'Timestamp Generator' same as 'platform bus clock '?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In Vybrid F-Series, is the clock frequency of 'Timestamp Generator' same as 'platform bus clock '?

ソリューションへジャンプ
1,069件の閲覧回数
高尾浩司
Contributor I

Hi, I want to evaluate Timestamp Generator and conduct an investigation into Timestamp Generator in Vybrid(VF6XX).

In Vybrid F-Series, is the clock frequency of 'Timestamp Generator' same as 'platform bus clock '?

ラベル(1)
タグ(1)
1 解決策
904件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Dear user,

Vybrid contain A5 with ETM from ARM so it is really ARM question. Nevertheless in ARM Information Center in CoreSight ETM-A5 Technical Reference Manual in chapter 2.3.1. Clock signals  is written "This must be the same clock as that wired to the CLKIN input of the Cortex-A5 processor." So we can say that timestamp is clocked by Vybrid A5 clock not platform clock.

ETM general info http://arm.com/products/system-ip/debug-trace/trace-macrocells-etm/index.php

Coresight on A5 link http://arm.com/products/system-ip/debug-trace/coresight-for-cortex-a.php there is button to get more information.

/Jiri

元の投稿で解決策を見る

1 返信
905件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Dear user,

Vybrid contain A5 with ETM from ARM so it is really ARM question. Nevertheless in ARM Information Center in CoreSight ETM-A5 Technical Reference Manual in chapter 2.3.1. Clock signals  is written "This must be the same clock as that wired to the CLKIN input of the Cortex-A5 processor." So we can say that timestamp is clocked by Vybrid A5 clock not platform clock.

ETM general info http://arm.com/products/system-ip/debug-trace/trace-macrocells-etm/index.php

Coresight on A5 link http://arm.com/products/system-ip/debug-trace/coresight-for-cortex-a.php there is button to get more information.

/Jiri