IAR Embedded debug problem with OpenSDA Pemicro on vybrid tower

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IAR Embedded debug problem with OpenSDA Pemicro on vybrid tower

Jump to solution
3,378 Views
ahmedrida
Contributor III

Hello everyone,


I'm a new owner of a tower kit vf65gs10, and I'm trying to compile a simple MQX hello example on IAR Embedded, but I'm getting some problems to make it.


I have already compile all the libraries as mentionned in the getting started guide with IAR.


I've also installed the firmwares of Pemicro, I put the board in bootloader mode then I drag and drop the cmsis-dap file.

I don't know exactly wich file I'm supposed to put in the bootloader.


I configure IAR options as following :

- Debugger -> PEMicro

- Run to main

- Attach to running target


Then I click debug and I have several messages depending on the configurations I put but it never works :

commerr.png

debuglog.png

Or sometimes this one when I try to run the example on A5 Core of m board :

autodetec.png

But when I hit Connect that only reset my board and I still can't connect to debug.

I really don't know how to solve this, anyone can help me ?


Thank you in advance.


Ahmed

0 Kudos
Reply
1 Solution
2,976 Views
timesyssupport
Senior Contributor II

Hi Ahmed,

We do not support the 3rd party IAR Embedded software. The following document contains our process for debugging MQX/Linux applications with Vybrid using DS-5:

https://linuxlink.timesys.com/docs/lab_notes_for_webgl_mcc_accelerometer_demo#Exercise-5-Debugging

Thanks,

Timesys Support

View solution in original post

0 Kudos
Reply
4 Replies
2,976 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g  Vybrid Processors ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community. 

0 Kudos
Reply
2,976 Views
ahmedrida
Contributor III

I moved it thank you.

Still stuck if anyone have an idea.

Ahmed

0 Kudos
Reply
2,976 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 Kudos
Reply
2,977 Views
timesyssupport
Senior Contributor II

Hi Ahmed,

We do not support the 3rd party IAR Embedded software. The following document contains our process for debugging MQX/Linux applications with Vybrid using DS-5:

https://linuxlink.timesys.com/docs/lab_notes_for_webgl_mcc_accelerometer_demo#Exercise-5-Debugging

Thanks,

Timesys Support

0 Kudos
Reply