I have u-boot running on the VF610TWR board. It boots from the SD Card. I want to disable it looking for the MT29F2G16ABA NAND chip. How does one do that?
I have a new board based on the vf610twr design (SD Card boot), but it doesn't have NAND flash. When I try to boot this new board, I get this from u-boot:
U-Boot 2013.07 (Aug 14 2014 - 07:45:53)
CPU: Freescale Vybrid 600 family rev1.2 at 396 MHz
Reset cause: POR
Board: TWR-VF65GS10
DRAM: 128 MiB
WARNING: Caches not enabled
NAND:
It *hangs* on the "NAND:" line. Since I don't have flash on this new board, I need to disable searching for it. Boot is from SD Card.
I'm going to try adding this line in the u-boot-2013.07/u-boot-2013.07/board/freescale/vf610twr\imximage.cfg file:
#unset CONFIG_CMD_NAND
but I have a feeling it isn't going to help...
Thanks
解決済! 解決策の投稿を見る。
 
					
				
		
Hello Jack,
You will want to modify your U-Boot board configuration header in order to configure out NAND boot support.
For example, if you are configuring U-Boot to build the vf610twr target, the board configuration header is located at include/configs/vf610twr.h in U-Boot source. You will want to comment out or remove line 74:
#define CONFIG_CMD_NAND
Then, you can rebuild (if you are building with Factory, you can run 'make u-boot-restage && make' to rebuild).
Thanks, and let me know if you have any questions.
Timesys Support
I just tried the '#unset CONFIG_CMD_NAND' and U-Boot still looks for NAND. So that #undef does nothing.
 
					
				
		
Hello Jack,
You will want to modify your U-Boot board configuration header in order to configure out NAND boot support.
For example, if you are configuring U-Boot to build the vf610twr target, the board configuration header is located at include/configs/vf610twr.h in U-Boot source. You will want to comment out or remove line 74:
#define CONFIG_CMD_NAND
Then, you can rebuild (if you are building with Factory, you can run 'make u-boot-restage && make' to rebuild).
Thanks, and let me know if you have any questions.
Timesys Support
 
					
				
		
 alejandrolozan1
		
			alejandrolozan1
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
I found that very helpful. Thank you!
Regards,
Alejandro
So when U-Boot comes up, it says this:
CPU: Freescale Vybrid 600 family rev1.2 at 396 MHz
I thought the U-boot set the A5 CPU at 500 MHz. Is U-Boot reporting a wrong value? It does this on both the Vybrid Tower and our new board.
Thanks.
 
					
				
		
Hello Jack,
I guess it is set for 396 MHz to make it possible to use the same code for both Consumer (500 MHz max.) and Automotive (400 MHz max.) parts. Who needs it to be higher for the Consumer part adjusts it "manually".
It is definitely better that having 500 MHz in the code and an avalanche of the "does not work!" field requiests from those using an Automotive part!
Sincerely, Naoum Gitnik.
I'm looking at the vf610twr.c file. What changes would I need to crank up the CPU clock speed from 396 MHz to 500 Mhz?
Thanks.
 
					
				
		
Hello Jackm
Have you looked at the How to set VF61 CPU A5 core speed to 500 MHz under Timesys Linux ? thread - there might be good hints for you in there.
Sincerely, Naoum Gitnik.
Thank you!
Thanks. I'm going to crank it up to 500 MHz and see what happens (MVF61 part)....
 
					
				
		
Hello Jack,
This is not an incorrect value as far as I am aware. The CCSR and CACRR registers which control this value are set in board/freescale/vf610twr/vf610twr.c. This line is printed by arch/arm/cpu/armv7/vf610/generic.c, which reads the CCSR and CACRR registers.
Thanks,
Timesys Support
Found that.....works! It skips nand_init() in board.c and loads. Then Linux comes up and I get the command prompt and all is good.
Thanks
 
					
				
		
Hello Jack,
(Please, also take a look at the Can I get working sources of U-BOOT 2013.07, nand? thread to see if it is anyhow related to your issue.)
[timesyssupport, may you comment here, please?]
Sincerely, Naoum Gitnik.
I blew the BT_FUSE_SEL fuse in OCOTP_CFG5 (OTP Bank0 Word6) and changed the BOOT_CFG1 byte in OCOTP_CFG4 to be 0x60 (sd card, fast mode, High SD Speed). We also checked the BOOTMOD pins (which are ignored anyway after fuse setting) and they were both low.
I'll check out the new U-Boot release to see if it has something critical that we need.
Thanks