HAB with QuadSPI XIP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,369件の閲覧回数
adamszalkowski
Contributor II

When booting on a VF6 using HAB, the Authenticate Data command fails with reason HAB_INV_ADDRESS.

Does HAB not support boot from QuadSPI with XIP?

The exact command was:

CA 00 14 00 // CMD_AUTHENTICATE

02 C5 00 00 // KEY=2, PRT=CMS, ENG=ANY

00 00 0A 74 // rel. addr of signature

20 00 00 00 // block1 address to verify

00 03 DC 00 // block1 length

Any ideas?

ラベル(1)
1 解決策
4,880件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
4,881件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
4,883件の閲覧回数
cyborgnegotiato
Senior Contributor II

Hi Adam,

As I know, Vybrid has HABv4 which support XIP.

Are you sure with this HAB_INV_ADDRESS fail reason? (just for information)

HAB_INV_ADDRESS mean you have some problem with address, for more information see the HAB4_API documentation.

00 00 0A 74 // rel. addr of signature

Could you check this relative address? Is it correct?

Utkarsh Gupta could you suggest more?


Regards,

Jozef

4,883件の閲覧回数
utkarsh_gupta
NXP Employee
NXP Employee

Hello,

I agree with Josef. HAB_INV_ADDRESS issue occurs due to either misaligned target address or denied access to that address. Please check the regions of the image addresses being signed and IVT self or entry pointer is not null.

Thanks,
Gupta

4,883件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 件の賞賛
返信
4,883件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport do you have an update?

0 件の賞賛
返信
4,883件の閲覧回数
timesyssupport
Senior Contributor II

Hello Karina,

      We reviewed the Vybrid Security reference manual and see nothing helpful/relevant. Does the Freescale Vybrid team have any input on this?

Thanks,

Timesys Support

4,883件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

cyborgnegotiator can you  check this case and share your thoughts?

0 件の賞賛
返信
4,883件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Jozef Maslik any update?

0 件の賞賛
返信
4,883件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

utkarshgupta-b45806 can you    share your thoughts about this case?

0 件の賞賛
返信