FlexBus burst mode question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexBus burst mode question

ソリューションへジャンプ
1,062件の閲覧回数
johnfielden
Contributor IV

Hi, I've looked over the reference manual and have a couple of questions about the FlexBus.

The only bus timings I see appear to show that all Flexbus signals must be qualified with the FB_CLK.  Please confirm, Flexbus is not an asynchronous bus.

There are diagrams of 32 bit to 8 bit port burst (looks like 6 clocks min).  But, I'm interested in doing a 32 bit to 16 bit port bursts.  If I do 32 to 16, how many clock cycles is the access?  4?  5?

I was really hoping to burst several 32 bit words per cycles, but I don't see that listed.   I'm assumming that idea is not possible.

Thanks,

John Fielden

0 件の賞賛
返信
1 解決策
849件の閲覧回数
naoumgitnik
Senior Contributor V

Dear John,

1.

According to the '32.4.7 Signal transitions' section, the bus is synchronous:

These signals change on the rising edge of the FlexBus clock (FB_CLK):

• Address

• Write data

• FB_TS/FB_ALE

• FB_CSn

• All attribute signals

FlexBus latches the read data on the rising edge of the clock.

2.

May you refer me to the specific section and/or diagram that shows "32-bit to 8-bit port burst", please?

Sincerely, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
850件の閲覧回数
naoumgitnik
Senior Contributor V

Dear John,

1.

According to the '32.4.7 Signal transitions' section, the bus is synchronous:

These signals change on the rising edge of the FlexBus clock (FB_CLK):

• Address

• Write data

• FB_TS/FB_ALE

• FB_CSn

• All attribute signals

FlexBus latches the read data on the rising edge of the clock.

2.

May you refer me to the specific section and/or diagram that shows "32-bit to 8-bit port burst", please?

Sincerely, Naoum Gitnik.

0 件の賞賛
返信