Hi, I've looked over the reference manual and have a couple of questions about the FlexBus.
The only bus timings I see appear to show that all Flexbus signals must be qualified with the FB_CLK. Please confirm, Flexbus is not an asynchronous bus.
There are diagrams of 32 bit to 8 bit port burst (looks like 6 clocks min). But, I'm interested in doing a 32 bit to 16 bit port bursts. If I do 32 to 16, how many clock cycles is the access? 4? 5?
I was really hoping to burst several 32 bit words per cycles, but I don't see that listed. I'm assumming that idea is not possible.
Thanks,
John Fielden
已解决! 转到解答。
Dear John,
1.
According to the '32.4.7 Signal transitions' section, the bus is synchronous:
These signals change on the rising edge of the FlexBus clock (FB_CLK):
• Address
• Write data
• FB_TS/FB_ALE
• FB_CSn
• All attribute signals
FlexBus latches the read data on the rising edge of the clock.
2.
May you refer me to the specific section and/or diagram that shows "32-bit to 8-bit port burst", please?
Sincerely, Naoum Gitnik.
Dear John,
1.
According to the '32.4.7 Signal transitions' section, the bus is synchronous:
These signals change on the rising edge of the FlexBus clock (FB_CLK):
• Address
• Write data
• FB_TS/FB_ALE
• FB_CSn
• All attribute signals
FlexBus latches the read data on the rising edge of the clock.
2.
May you refer me to the specific section and/or diagram that shows "32-bit to 8-bit port burst", please?
Sincerely, Naoum Gitnik.