Failed to write 104.508 bytes to address 0x3F000000 while writing block of 4.096 bytes to address 0x3F000000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failed to write 104.508 bytes to address 0x3F000000 while writing block of 4.096 bytes to address 0x3F000000

2,500 次查看
hzekierdogan
Contributor II

Hi,

I am trying to build and debug pingpong demo of the MQX using DS-5 in windows. When I started a debug session after build , I got following errors during loading to image tower board. How can I fix this

Thanks

Zeki

Signals handled by operating system

Connected to stopped target Freescale - Vybrid VF6xx on TCP:localhost

Execution stopped at: 0x3F006716

0x3F006716   MOVS     r0,#2

set substitute-path "C:/Users/drebar01/Documents/Projects/Vybrid/WS_Vybrid_MQX/Vybrid_M4_BareMetal/" "C:\Users\drebar01\Documents\Projects\Vybrid\WS_Vybrid_MQX\Vybrid_M4_BareMetal\"

loadfile "C:\Freescale\Freescale_MQX_4_1_Vybrid\mqx\examples\hello\build\ds5\hello_twrvf65gs10_m4\int ram debug\hello_twrvf65gs10_m4.axf"

ERROR(CMD16-TAD274-NAL22):

! Failed to load "hello_twrvf65gs10_m4.axf"

! Failed to write 104.508 bytes to address 0x3F000000 while writing block of 4.096 bytes to address 0x3F000000

! General error on memory or register access.

cd "C:\Users\c001\Documents\DS-5 Workspace2"

Working directory "C:\Users\c001\Documents\DS-5 Workspace2"

set debug-from main

start

WARNING(CMD399-COR168):

! Failed to start the target

! No function named "main" could be found

WARNING(CMD407): Trying the entry point instead

ERROR(CMD426): Cannot find symbol to start or entrypoint, the file or load commands may be used to set the entrypoint

wait

break -d -p "C:\Users\drebar01\Documents\Projects\Vybrid\WS_Vybrid_MQX\Vybrid_M4_BareMetal\src\main_M4.c":44

WARNING(CMD452-COR167):

! Breakpoint 1 has been pended

! No compilation unit matching "C:/Users/drebar01/Documents/Projects/Vybrid/WS_Vybrid_MQX/Vybrid_M4_BareMetal/src/main_M4.c" was found

condition 1

break-script 1 ""

ignore 1 0

break-stop-on-cores 1

unsilence 1

Breakpoint 1 unsilenced

wait

continue

标签 (3)
0 项奖励
回复
4 回复数

1,745 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

alejandrolozano​ are you able to help?

0 项奖励
回复

1,745 次查看
alejandrolozan1
NXP Employee
NXP Employee

Sure Karina,

Zeki, I would start trying to download the ping pong demo first with the debugger and not loading Linux of the A5 and make sure that the demo starts correctly.

Do you have access to this link?

https://linuxlink.timesys.com/docs/wiki/engineering/userguide_vybrid_mcc#Building

It contains the steps to build and test the ping pong demo.

Best Regards,

Alejandro

1,745 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

hzekierdogan@hotmail.com​ did you get  previous comment?

1,745 次查看
hzekierdogan
Contributor II

Yes, But I couldn't find time to look this issue yet.

Thanks

0 项奖励
回复