FBx / fbcon rotation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,244件の閲覧回数
Nouchi
Senior Contributor II

Hello,

What is the best way to make frame buffer and console rotation working like this: echo 1 > /sys/class/graphics/fb0/rotate  ?

/sys/class/graphics/fb0/rotate exists, cat /sys/class/graphics/fb0/rotate return 0, but writing into it, turns the display in blac

Emmanuel

ラベル(5)
0 件の賞賛
返信
1 解決策
2,530件の閲覧回数
timesyssupport
Senior Contributor II

Hi,

It is a known issue that the DCU driver does not support rotation. We do not have an ETA for a fix at this time; if this is a time-sensitive issue, Timesys can pursue under a services agreement.

Thanks,

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,530件の閲覧回数
naoumgitnik
Senior Contributor V

Hello Emmanuel,

I am a bit confused - is it posted in the right Community space? If so, may you refer to a specific Vybrid document / clause / page, please?

Regards, Naoum Gitnik.

0 件の賞賛
返信
2,530件の閲覧回数
Nouchi
Senior Contributor II

Hello Naoum,

I'm working on a TWR-65GS10 kit with timeSys factory. I'm using a 7" WVGA(800*480) display, and it's positioned in portrait mode, so I need to rotate something, frame buffer, console and QT environment. For Qt it's easy, just use -display "transformed:rot90:1" option in command line, but for the frame buffer or console, it's not so easy, that why I ask some help about this.

The classic way to do that with linux is to use /sys/class/graphics/fb0/rotate for frame buffer rotation and /sys/class/graphics/fbcon/rotate for console rotation, and it doesn't work.

regards,

Emmanuel.

0 件の賞賛
返信
2,530件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you  attend this case?

0 件の賞賛
返信
2,531件の閲覧回数
timesyssupport
Senior Contributor II

Hi,

It is a known issue that the DCU driver does not support rotation. We do not have an ETA for a fix at this time; if this is a time-sensitive issue, Timesys can pursue under a services agreement.

Thanks,

Timesys Support

0 件の賞賛
返信
2,530件の閲覧回数
carlovalgocela
Contributor III

Hi,

Any updates on DCU driver supporting the framebuffer rotation?

0 件の賞賛
返信