Ethernet Switch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Switch

Jump to solution
4,978 Views
xueweiliu
Contributor I

When the Ethernet Switch will be supported in MQX?


Regards,

Liu Xuewei

Tags (2)
0 Kudos
Reply
1 Solution
4,583 Views
anthony_huereca
NXP Employee
NXP Employee

MQX wouldn't prevent you from using the switch, but there just wouldn't be code to enable and make use of the switch feature. MQX puts the switch in bypass mode.

View solution in original post

0 Kudos
Reply
4 Replies
4,583 Views
anthony_huereca
NXP Employee
NXP Employee

There is not a plan to support it in MQX. It is supported in Linux however.

https://linuxlink.timesys.com/docs/wiki/engineering/vybrid_release_notes

0 Kudos
Reply
4,583 Views
xueweiliu
Contributor I

Anthony,

IN the RM 46.1.2, "Can be configured to operate as a 3-port switch (switch mode) " and is it possible to use the switch working at this mode in MQX or without OS?

Thanks!

0 Kudos
Reply
4,584 Views
anthony_huereca
NXP Employee
NXP Employee

MQX wouldn't prevent you from using the switch, but there just wouldn't be code to enable and make use of the switch feature. MQX puts the switch in bypass mode.

0 Kudos
Reply
4,583 Views
xueweiliu
Contributor I

Thanks! But it's realy a hard work to write the driver for the switch by ourself. Do you have a plan to release the bare code for some basic funciton?

0 Kudos
Reply