Ethernet Switch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,976件の閲覧回数
xueweiliu
Contributor I

When the Ethernet Switch will be supported in MQX?


Regards,

Liu Xuewei

タグ(2)
0 件の賞賛
返信
1 解決策
4,581件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

MQX wouldn't prevent you from using the switch, but there just wouldn't be code to enable and make use of the switch feature. MQX puts the switch in bypass mode.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,581件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

There is not a plan to support it in MQX. It is supported in Linux however.

https://linuxlink.timesys.com/docs/wiki/engineering/vybrid_release_notes

0 件の賞賛
返信
4,581件の閲覧回数
xueweiliu
Contributor I

Anthony,

IN the RM 46.1.2, "Can be configured to operate as a 3-port switch (switch mode) " and is it possible to use the switch working at this mode in MQX or without OS?

Thanks!

0 件の賞賛
返信
4,582件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

MQX wouldn't prevent you from using the switch, but there just wouldn't be code to enable and make use of the switch feature. MQX puts the switch in bypass mode.

0 件の賞賛
返信
4,581件の閲覧回数
xueweiliu
Contributor I

Thanks! But it's realy a hard work to write the driver for the switch by ourself. Do you have a plan to release the bare code for some basic funciton?

0 件の賞賛
返信