Error when attempting to install 10.4 Microcontroller Drivers Suite in latest DS-5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error when attempting to install 10.4 Microcontroller Drivers Suite in latest DS-5

ソリューションへジャンプ
4,451件の閲覧回数
dachancellor
Contributor II

I just received my Vybrid Tower Kit.

I installed the latest version of DS-5 (5.22).

When attempting to install 10.4 Microcontroller Drivers Suite for Processor Expert support, the install fails.

An error occurred while installing the items

session context was:(profile=SDKProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=null --> [R]com.freescale.processorexpert.standalone_root 10.4.0, action=com.fresscale.updater.customactions.actions.FreescaleInstall).

org/eclipse/core/runtime/adaptor/LocationManager

org/eclipse/core/runtime/adaptor/LocationManager

The zip file for installing mentions Eclipse 3.7 and 4.2.

The latest version of DS-5 is Eclipse 4.4.2.

Is this the issue ?

Is there a version of the Microcontroller Drivers Suite that works in DS-5 (5.22) ?

Thanks,

Chandler

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
4,136件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Processor Expert Driver Suite v10.4 is only up to Eclipse Kepler. The 10.4 plugin installer does not run in Eclipse Luna (4.4) due a compatibility issue.

There is a plugin for Eclipse Luna (4.4), it is for Kinetis, not for Vybrid.

pastedImage_1.png

So this one should work with DS-5 (Luna based), but will not support Vybrid. And there are currently no plans to make an update for Vybrid. So if you are using Vybrid with DS-5 with Processor Expert, you have to use pre-4.4 Eclipse.

Best regards,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,136件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I do not know how you are trying to install PE. But the driver suite is delivered and installed as a comprehensive product with the Eclipse 4.2 (Juno) IDE. It is also available as an Eclipse plug-in for existing Eclipse 3.7 (Indigo) and Eclipse 4.2 (Juno) installations. I do not think it can be installed as a plug-in in DS-5.

Best Regards,

Alejandro

0 件の賞賛
返信
4,136件の閲覧回数
dachancellor
Contributor II

Alejandro,

I was using the provided Plugins to install into DS-5, PExDrv 10.4 and 10.4 Update 3.

I installed an older version of DS-5 which runs Eclipse 3.7 (5.17.1), and the plugin installation worked fine.

My question was if there were any updated plugin files or plans to support the later versions of DS-5, which run Eclipse 4.4+

Also, you are correct that the driver suite runs fine as a standalone Eclipse 4.2 IDE capable of generating PE code.

V/r,

Chandler

0 件の賞賛
返信
4,136件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I looked for information regarding the PE roadmap but I had no success. BlackNight​ sorry to trouble you, I wonder if you have information that may help.

Best Regards,

Alejandro

0 件の賞賛
返信
4,137件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Processor Expert Driver Suite v10.4 is only up to Eclipse Kepler. The 10.4 plugin installer does not run in Eclipse Luna (4.4) due a compatibility issue.

There is a plugin for Eclipse Luna (4.4), it is for Kinetis, not for Vybrid.

pastedImage_1.png

So this one should work with DS-5 (Luna based), but will not support Vybrid. And there are currently no plans to make an update for Vybrid. So if you are using Vybrid with DS-5 with Processor Expert, you have to use pre-4.4 Eclipse.

Best regards,

Erich

0 件の賞賛
返信
4,136件の閲覧回数
dachancellor
Contributor II

Thanks Erich !

0 件の賞賛
返信