Enabling the L2 switch with device tree

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enabling the L2 switch with device tree

2,059 次查看
dustind
Contributor I

Hi,

 

I'm trying to enable the L2 switch (in switch mode) on my PHYTEC phyCORE Vybrid Development Kit (uses the VF610). I've downloaded the 3.13 Kernel from Timesys and applied the patch linux-3.13.9-vybrid-ts2.5.patch. The 3.13 kernel uses a device tree to configure the board and I've attached the dts file I'm using.

 

In the kernel, I changed the two configuration options as outlined here: How to use L2 switch on Vybrid processor ?

 

When I boot I see:

...

400d0000.ethernet supply phy not found, using dummy regulator

fec 400d0000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00

fec 400d0000.ethernet (unregistered net_device): Using random MAC address: 9a:2e:e4:90:25:50

libphy: fec_enet_mii_bus: probed

400d1000.ethernet supply phy not found, using dummy regulator

fec 400d1000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00

fec 400d1000.ethernet (unregistered net_device): Using random MAC address: de:d4:f5:7b:4f:2d

libphy: fec_enet_mii_bus: probed

Ethernet Switch Version 1.0

...

Configuring network interfaces: fec 400d0000.ethernet eth0: Freescale FEC PHY driver [Micrel KSZ8051] (mii_bus:phy_addr=400d0000.etherne:00, irq=-1)

...

libphy: 400d0000.etherne:00 - Link is Up - 100/Full

 

 

Running an ifconfig after boot reveals:

eth0  Link encap:Ethernet  HWaddr 04:2D:F4:05:5A:45
      inet addr:10.11.65.15  Bcast:0.0.0.0  Mask:255.255.0.0
      UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
      RX packets:110 errors:0 dropped:0 overruns:0 frame:0
      TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
      collisions:0 txqueuelen:1000
      RX bytes:9509 (9.2 KiB)  TX bytes:0 (0.0 B)

 

lo    Link encap:Local Loopback
      inet addr:127.0.0.1  Mask:255.0.0.0
      UP LOOPBACK RUNNING  MTU:65536  Metric:1
      RX packets:0 errors:0 dropped:0 overruns:0 frame:0
      TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
      collisions:0 txqueuelen:0
      RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

I have a cable connecting eth0 to my router and I can ping other devices on the network. However, when I plug another device (for example a raspberry pi) into eth1 there is no traffic between the board and the device and the LEDs on eth1 show no activity. Does anyone know how to enable the switch?

Original Attachment has been moved to: pcm052.dts.zip

标签 (2)
0 项奖励
回复
2 回复数

1,172 次查看
timesyssupport
Senior Contributor II

Hello Dustin,

We have had other reports of issues with the L2 switch on Phytec Vybrid with the 3.13 kernel; we are investigating, but as Phytec provides the kernel support for their hardware, they are better suited to accurately address this issue. Should anything relevant come of our efforts, we will follow up.

Thanks,

Timesys Support

1,172 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you attend this case?

0 项奖励
回复