EEPROM SPI component in Processor expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEPROM SPI component in Processor expert

2,501件の閲覧回数
markwatson
Contributor III

We are attempting to use the AT25HP512 PEX component, but it is complaining about not being able to find EEPROM_SPI.  Does anyone know where I can find that driver?

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

2,009件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello Mark,

I suppose that you are using the AT25HP512 component from the mcuoneclipse web pages. You can find all source code files on the git repository ErichStyger/mcuoneclipse · GitHub

If you are not able the use the AT25HP512 component you can have an old version or damaged installation of this component in your PEx installation.

I would recommend that you should install the whole package (part1 and part2) from PEupd folder (see mcuoneclipse/PEupd at master · ErichStyger/mcuoneclipse · GitHub).

If you still have a problem with this component contact the author of the component, please. You can use the Issues · ErichStyger/mcuoneclipse · GitHub page and submit a new issue.

Best Regards,

Marek Neuzil


2,009件の閲覧回数
markwatson
Contributor III

Thank you for the information.  In the end I did not use PEX, but used the code in C:\FreeScale\Freescale_MQX_4_1\mqx\examples\spi\spi_memory.c with minor modifications.

0 件の賞賛
返信

2,009件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

PetrZeman can you attend this case?

0 件の賞賛
返信

2,010件の閲覧回数
PetrZeman
NXP Employee
NXP Employee

I'm really sorry, but I'm surely not the right person for this topic, anyway.. do you know what source that PEX component comes from? I'll forward this case to my colleagues, they might know more.

0 件の賞賛
返信